MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS3DH simultaneous free-fall interrupt and normal XYZ operation

HiIs it possible to configure the interrupt function for free-fall with normal XYZ polled operation, or is it better to use the interrupt in low power mode and performing the free-fall via normal XYZ programmatically in normal operation?Thanks! 

rep by Associate II
  • 582 Views
  • 4 replies
  • 2 kudos

Resolved! About Embedded compensation for ASM330LHH

Regarding the statement in the ASM330LHH datasheet “Embedded compensation for high stability over temperature”, does this mean that each output is temperature compensated? Does the compensation value correspond to the memory contents loaded when the ...

ggob by Associate III
  • 428 Views
  • 2 replies
  • 0 kudos

LSM6DSOX high power consumption

Hello, I recently integrated LSM6DSOX on a testing PCB which contains an MCU and some other peripherals. The problem is that I have been trying to reduce power consumption without success, and I thought maybe you could help me find the problem. First...

dimitra by Associate
  • 248 Views
  • 1 replies
  • 0 kudos

LSM6DSO using both of SPI/I2C

Hello, I am designing a PCB board using LSM6DSO and STM32f1xx, this PCB design will be only an experimental design for a bigger project, so I need both SPI and I2C to be available for testing (not at the same time).I'm wondering if there will be any ...

Screenshot (34).png

strange problem with lsm6dsv320x HG accelerometer

HiWe are testing out the lsm6dsv320x, which will be used on our new board.The low G accelerometer is working fine, however the high G looks to be reporting wrong values.If I use a simple calculation to computer the angles, the high G  is off by about...

richardp by Associate
  • 171 Views
  • 1 replies
  • 0 kudos

STEVAL-MKI248KA availability

Hi everyone.Can someone from ST please provide information about when the STEVAL-MKI248KA will be available for testing?We are currently designing a new device that could really benefit from ISM6HG256XTR but we are tight on time and already in the in...

Resolved! Need thermal details for STM IC's

Hi team,We need thermal details (Junction to ambient temperature, Case temperature and body temperature) for the following IC's:ASM330LHHXG1TRM24M02-DWMN3TP/KPlease provide the details for the given IC's.Thanks & regards,Aravind R