cancel
Showing results for 
Search instead for 
Did you mean: 

Errors in the configurator of the STM32CubeIDE for microcontroller STM32L100RB. (Not observed for STM32F103, etc.) (Low Layer only)

ATret.3
Associate III

Ubuntu STM32CubeIDE 1.8/1.7

File -> New -> STM32 Project

Choose STM32L100RB -> Next -> Project Name : "removeMe2" -> Finish

In Device Configuration Tool:

  Pinout&Configuration -> Connectivity -> SPI1 -> Mode: Full Duplex Master

  Project Manager -> Advanced Setting -> Driver Selector -> SPI: LL

Save and generate code.

Project -> Build All

.........

./Core/Src/main.c: In function 'MX_SPI1_Init':

../Core/Src/main.c:210:3: warning: implicit declaration of function 'LL_SPI_SetStandard' [-Wimplicit-function-declaration]

 210 |  LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);

   |  ^~~~~~~~~~~~~~~~~~

........

Build Failed. 3 errors, 0 warnings. (took 901ms)

And I can't open declaration (Hotkey - F3) of LL_SPI_SetStandard(). (For other functions IDE try to open *.c file at first, but not *.h. Definition of LL_SPI_SetStandard() in the stm32l1xx_ll_spi.h)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ATret.3
Associate III

Error in library.

#if defined(SPI_CR2_FRF)
/**
  * @brief  Set serial protocol used. TI Mode not supported for Category 1 and 2.
  * @note   This bit should be written only when SPI is disabled (SPE = 0) for correct operation.
  * @rmtoll CR2          FRF           LL_SPI_SetStandard
  * @param  SPIx SPI Instance
  * @param  Standard This parameter can be one of the following values:
  *         @arg @ref LL_SPI_PROTOCOL_MOTOROLA
  *         @arg @ref LL_SPI_PROTOCOL_TI
  * @retval None
  */
__STATIC_INLINE void LL_SPI_SetStandard(SPI_TypeDef *SPIx, uint32_t Standard)
{
  MODIFY_REG(SPIx->CR2, SPI_CR2_FRF, Standard);
}
 
/**
  * @brief  Get serial protocol used
  * @rmtoll CR2          FRF           LL_SPI_GetStandard
  * @param  SPIx SPI Instance
  * @retval Returned value can be one of the following values:
  *         @arg @ref LL_SPI_PROTOCOL_MOTOROLA
  *         @arg @ref LL_SPI_PROTOCOL_TI
  */
__STATIC_INLINE uint32_t LL_SPI_GetStandard(SPI_TypeDef *SPIx)
{
  return (uint32_t)(READ_BIT(SPIx->CR2, SPI_CR2_FRF));
}
#endif

Adding next simbols in the Project -> Properties -> C/C++ General - >Path and Symbols -> Symbols solves the problem (I think, it should be in CMSIS).

0693W00000HorTjQAJ.png