cancel
Showing results for 
Search instead for 
Did you mean: 

I use NucleoL152RE with interrupt on PC13. Checking the ISER in the SFR, I have the address 0xE000E004 but the base address is 0xE000E100. When I check in the memory browser at 0xE000E104, I get the right ISER value. Thanks to confirm the bug of cubeIDE

JMene.1
Associate III
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
LaurentL
ST Employee

Hello,

Thanks for reporting this issue.

You can check NVIC registers in Cortex-M3 registers in SFR view. (above STM32L151).

Cortex-M3 svd file has been fixed for ISERx regs in STM32CubeIde 1.7.0

NVIC regs should be removed from STM32L151 svd file I suppose if there is an error.

Rgds,

Laurent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.