I cannot import file in Workspace
I put this folder in the workspace with all the other projects:Now I have to import it as I have always done: file - import - existing projects in the workspaceI cannot press on "finish"
I put this folder in the workspace with all the other projects:Now I have to import it as I have always done: file - import - existing projects in the workspaceI cannot press on "finish"
Hi, I tryed differents issues to solve my probleme, include this :https://stackoverflow.com/questions/72564141/why-is-my-stm32f407-not-being-recognized-by-computer-windows-10 https://stackoverflow.com/questions/71678792/st-link-v2-detected-as-usb-mas...
Hello,I am working on a project that requires the code to be stored in the external QSPI flash but the problem is, I have no idea how the external memory loader generated by CubeMX works. I have tried following this article, but the external loader l...
Hello forum,I'm trying to use the BSP driver while implementing a USB Host functionality. after the initiation of everything the USB needs, the BSP started to raise a lot of errors of undeclared/undefined stuff, after checking I saw that the error wa...
CubeIDE 1.16.0 and/or CubeMX 6.12.0.STM32H563 - SPI devices 4, 5, and 6 only support data widths of 8 or 16 bits. IDE/MX have a Data Size dropdown that let you choose 4 - 16 bits. Widths other than 8 or 16 blow up in HAL_SPI_Init when the data width ...
I'm trying to communicate with external device using SPI, but I'm not getting any SPI peripheral clock at configuration level and there is no clock initialization details in SPI Init(); void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi){GPIO_InitTypeDef G...
Hello, i used to have an arduino + NRF24L01 communicating with a raspberry pi, wich worked without any issues.I dont have much knowledge in this area, and due to the lack of documentation in communicating these devices using nrf24, i find myself at a...
Can someone please shed some light on why opening an .ioc file on Linux is like Russian roulette. Sometimes it works, sometimes you get a blank screen, sometimes nothing at all and sometimes 'Yes!!! it's working'.Running IDE 1.16.0 on Linux Mint 21.3...
Hello!I have an issue when creating a new project through STM32CubeIDE.I use the application on Windows, it is STM32CubeIDE v1.16.0 and I try to work on an STM32H563ZI.I installed it off line (security constraints preventing any network connection) s...
Hi all,If I recall correctly, CubeIDE V1.8 was very unstable when using the integrated MX, with many of the control components failing to redraw correctly, or not at all. Sometimes you could trick it into drawing by minimising and restoring the form....