WS2813B-Mini / STM32F103C8T6
Hello everyone, There are 24pcs WS2813-Mini led on my PCB. I didn't set these with timer. How can I drive the WS2813-Mini led with STM32F103C8T6 in STM32CubeIDE?Thanks.
Hello everyone, There are 24pcs WS2813-Mini led on my PCB. I didn't set these with timer. How can I drive the WS2813-Mini led with STM32F103C8T6 in STM32CubeIDE?Thanks.
Dear all,Could not verify ST device!This error popped up suddenly and blocks any progress. I took an older computer and had the same error again.Therefore, I suspected a hardware failure and ordered new adapters and processor boards, but I kept havin...
Hello, Recently I have purchased an evaluation board "NUCLEO-G071RB" to program/debug our custom board using ST-LINK. After 4 time successfully attemps to program our custom board, the evaluation board came with follow error and it was impossible to ...
Hello, I get the following error when I debug with blue pill. see the attached picture How can i fix that? thank you in advance
I have the x-nucleo-GFX01M2 LCD which is compatible with my nucleo 64 board (F103RB). I am wondering how best to get started with graphics on this LCD, as there are no examples in the X Cube Display 3.0.0. for this board. The examples are for some G,...
Hello,for a DIY project including LoRa ra-02, MPU6050 and NEO-6M i have purchased some Blue pills from a vendor but it turned out they are fake blue pills (STM32F103C6).I am trying to make a RC, so i have a Transmitter which needs 2xSPIs (one for LoR...
Hi, I have a question to the ST community. I'm currently working on a project including an ECU form a diesel engine. The ECU uses J1939 for communication. I need to be able to read messages en send to the ECU. To do that I'm using an STM3210E-EVAL. I...
I'm having an issue using STM32CubeIDE to program my blue pill boards. I get the below error each time. Error in final launch sequence:Error in initializing ST-LINK device.Reason: (18) Could not verify ST device! Abort connection.Error in initializ...
We're planning on using an STM32103RET6 with an external 10K pull up to VDD (3.3V). Can the STLINK-V3SET drive the combination of the internal pull up (30K-50K) and the external 10K resistance on the NRST pin?
I've been asked to write some firmware for a legacy board that has an STM32F102CBT6 mcu on it.I have been involved in other computer and mcu projects over the years, but not with an STM32F. I'd like to get up to speed by starting on some basic progra...