Dear Sir.Attached a code of SystemClock_Config();void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (...
Dear Sir.Attached a schematic of STM32U585 . LDO_V28 is tested for 2.8v.Issuing the commandHAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE); HAL_SYSCFG_VREFBUF_VoltageScalingConfig(SYSCFG_VREFBUF_VOLTAGE_SCALE2); HAL...
Setup is as follows:ADC1 & 2 in 'Dual regular simultaneous mode only'DMA1 stream 0 used to transfer ADC data to AXI SRAM buffer (40000 32 bit values), DMA circular mode.Using 'HAL_ADC_ConvHalfCpltCallback' to signal half buffer filled and 'HAL_ADC_Co...
hellow.I tried to read multiple adc using stm32h743, but I had great difficulty due to inter-channel interference.I tried to read multiple adc using a simpler "NECTULEO-L073RZ" to find out what the problem was, but the same problem occurred.Please he...
I've been working on some code to control a 4-wire touchscreen on DisplayTech's DT028BTFT-TS using timers to de-bounce the respective touch screen wires.The code works on the Nucleo-F413ZH under debug and standalone. The coordinates of the positioned...
Hello, I am struggling finding electrical peripherals interconnection information for STM32F469. Peripherals are not covered in the datasheet, and I have looked thru Application Notes to best of my ability. Is there a document I missed that goes over...
Dev board: Nucleo-F767ZIDear all,as I wanted to have my own Vref+ for ADC conversions I removed solder bridge SB12 (coupling Vref+ with VDD) to input my own reference voltage (~3V) at Pin 6 CN7.After removing the SB12 however the STM 32 device is not...
Hello. A have my custom board with STM32G431CBU microcontroller. Power domain on my board are shown in the picture:I want to measure the voltage on Vref+ pin. The analog domain settings of CubeMX are:The code for single ADC acquisition:HAL_ADC_Start(...