STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo H723ZG docking options

Hello,I want to use the Nucleo H723ZG for a project with analog & digital lines and can't find the article number of the headers CN7, CN8, CN9, CN10. Is there a specific cable/contact type I can use to plug in the black header body? Or are the header...

STM32L431 DAC

Which DAC method is used for STM32L431, R-2R or resistor strings?Different things are written in the two materials. https://www.st.com/content/ccc/resource/training/technical/product_training/01/4b/81/0e/21/a6/4c/55/STM32L4_Analog_DAC.pdf/files/STM32...

kazuchib by Associate II
  • 992 Views
  • 6 replies
  • 0 kudos

Which is the best stm32 board (nucleo or evaluation) with embedded high performance DAC for sinusoidal signal generation? see next details.

I am looking for a microcontroller board for the following application:Receive a square wave LVDS signal at 1 kHz (more or less) and generate 2 sinusoidal single-ended output with the same frequency of the incoming square wave with the highest resolu...

Tommino by Senior
  • 912 Views
  • 4 replies
  • 0 kudos