STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 ST-LINK Utility Programming error

Posted on May 17, 2018 at 14:24Hi everyone,I have a very strange behavior using the STM32 ST-LINK Utility v4.2.0.0. While flashing a specific HEX file, the error message 'Programming error @ 0x08008C00' is occuring.When I use the uVision Keil Flash ...

ame by Associate II
  • 1120 Views
  • 2 replies
  • 0 kudos

Greyed interface in ST-Link Utility

Posted on April 11, 2018 at 17:05Hello everyone, I am having issues with ST-Link utility. Whenever I first launch it, everything looks fine, but if I try to change something in the settings (such as 'connect under reset') and then I press OK, the se...

B C by Associate II
  • 1221 Views
  • 12 replies
  • 0 kudos

[STM32] No voltage on VDD_TARGET pin

Posted on April 12, 2018 at 23:51I have a microcontroller (STMF103RET) mounted to the adapter. I would like to program it using the ST-Linkv2 programmer from the Nucleo board (STM32F103RB). According to the instructions, I disconnected the CN2 jumpe...

0690X00000604ZiQAI.jpg 0690X00000604ZnQAI.jpg
bastik * by Associate
  • 555 Views
  • 1 replies
  • 0 kudos

STM32F103 - Read Out Protection

Posted on April 19, 2017 at 16:43Hi,is it possible to enable Read Out Protection without power reset after it?Problem description: after setting Read Out Protection option enabled (by the STM32 ST-LINK Utility) the microcontroller does not reset. Mo...

Kaza K by Associate II
  • 313 Views
  • 2 replies
  • 0 kudos

iNemo SWD programming problem

Posted on April 15, 2015 at 19:50Hi to all, I'm trying to program my iNemo based custom board with the ST LINK provided with the STM32F4 Discovery. When I try to connect with STM32 ST-Link Utility I get the error: '' Core is held in reset''. Another...

daniel23 by Associate II
  • 272 Views
  • 1 replies
  • 0 kudos