Mbed firmware updater - can it load to RAM?
Could anyone point me to a good description of the Mbed firmware update feature of ST-LINK, via "USB disk"?What image formats does it accept?Can it load (and run) images located in internal RAM?
Could anyone point me to a good description of the Mbed firmware update feature of ST-LINK, via "USB disk"?What image formats does it accept?Can it load (and run) images located in internal RAM?
The Nucleo we are using has build in ethernet module.
Yesterday, while debugging in mBed, I experienced strange problems like being unable to debug, unless i unplug and replug the board. Maybe unrelated.Today, the board is not recognized (USB descriptor problem it seems).
Several Nucleo boards come with an embedded stlink V2-1 which supports MBED programming by copying the firmware binary to a USB mass storage device. If the programmer is snapped off the board and put in to external mode, does this method of programmi...
I have been doing a lot of reading lately about the flashing process and bootloaders and not everything is clear.The datasheet of my microcontroller says that it is stlink that enables mbed. I have confirmed that I have to upload via stlink in order ...