STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Backward compatibility

Hi, for our development we have selected "STM32F207ZG". The eval board which I see for MCU is "NUCLEO-F207ZG", which has pin-outs but not the required hardware interfaces on-board (usb-c fs, micro-sd, lcd, fsmc).The dev board "32F469IDISCOVERY" has s...

GauravK by Associate
  • 128 Views
  • 9 replies
  • 4 kudos

STM32f207's MII with Marvel's MII

Hi All,     I'm developing a project, in which I've connected the MII port of STM32F207 with Marvel IC 88E6060 (Ethernet + fiber switch) MII port 5 but the firmware support (SPL for STM32F2XX) provides libraries for DP83848 PHY only.      Hence, if I...

External circuitry for voltage regulator pins (VCAP) and software configuration using HAL layer for STM32F207ZG device.

Dear all, I'm facing the firmware downloading on a custom board for the first time after its testing version was produced.  This custom board design was an heritance from an externarl designer but I have found some hardware issues that must be fixed....

0693W00000Y8keEQAR.jpg
genisuvi by Associate III
  • 793 Views
  • 8 replies
  • 0 kudos