Skip to main content
PZwar
Associate
Oct 14, 2019 2:09 PM UTC
Question

How to deal wirh : Could not verify ST device! ?

Dear all,

Could not verify ST device!

This error popped up suddenly and blocks any progress. I took an older computer and had the same error again.

Therefore, I suspected a hardware failure and ordered new adapters and processor boards, but I kept having the same error again.

I have upgraded the STM32CubeIDE, the st-link drivers (dpinst_amd64.exe) and st-stlink-server(st-stlink-server.1.1.1-3.msi).

The st_link v2 adapter have been upgraded with the latest firmware.

Using STM32 Link Utility, I was able to program, verify and run blink applications.

I am using BluePills (STM32F103C8) with chinese adapters on a 64 bit Windows 10 machine.

Please find below the output produced when starting debugging in STM2CubeIDE using the GDB server in SWD mode.

I also selected the OPENOCD debugger, but it also failed, though in a different way.(see below)

Does anyone have a suggestion how to proceed on this?

Cheers, Paul

..........................ST-LINK GDB server.....................

STMicroelectronics ST-LINK GDB server. Version 5.2.3

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    LogFile Name        : C:\Users\Paul_2\Documents\STM32\Workspace\test\Debug\st-link_gdbserver_log.txt

    Logging Level       : 31

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Enabled

    SWD Debug         : Enabled

Hardware watchpoint supported by the target 

SWD frequency = 4000 kHz

ST-LINK Firmware version : V2J31S7

Device ID: 0x410

PC: 0xc6640804

ST-LINK device status: HALT_MODE

ST-LINK detects target voltage = 3.17 V

Vendor = 0x55 

Error in initializing ST-LINK device.

Reason: ST-LINK: Could not verify ST device! Abort connection.

......................OPENOCD.........................................

Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-23-20:37)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 8000 kHz

adapter_nsrst_delay: 100

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 8000 kHz

Info : STLINK v2 JTAG v31 API v2 SWIM v7 VID 0x0483 PID 0x3748

Info : using stlink api v2

Info : Target voltage: 3.166882

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Stlink adapter speed set to 4000 kHz

Warn : UNEXPECTED idcode: 0x2ba01477

Error: expected 1 of 1: 0x1ba01477

in procedure 'init' 

in procedure 'ocd_bouncer'

This topic has been closed for replies.

17 replies

Oct 15, 2019 6:22 AM UTC

Hi !

I am not very fluent in SWD, but the verbose output from Open OCD helps to identify the issue : the ID read by both tools differs from what is expected. Meaning that the error is the same in both cases.

Your device under test reads back 0x2ba01477 while the tools expect 0x1ba01477. I don't think it can be an electrical problem. Since you are using a bluepill, maybe the microcontroller is a counterfeit product. You should ST about this, perhaps with a picture of the uC.

PZwar
PZwarAuthor
Associate
Oct 17, 2019 11:50 AM UTC

Could not verify ST device!

Thank you so much, Kraal!

I inspected the looks of the chip and found it quite different from the ones I used before.

The text was not engraved but printed in a sloppy way. I think that your suggestion of a counterfeit is right.

I tried to make these counterfeits working under STM32CUBEIDE and OpenOCD.

Therefore, I adapted the st_scripts/target/stm32f1x.cfg file by replacing the 0x1ba01477 by 0x2ba01477.

I also added a line:

reset_config trst_only

This gives a error message:

Error: BUG: can't assert SRST

Neverthless, I could load and debug my code.

SWadi.1
Visitor II
Mar 16, 2020 8:44 PM UTC

Hi PZwar,

I have the same problem.

However I am unable to locate the "st_scripts/target/stm32f1x.cfg" file or folder on windows 10.

Using STM32CUBEIDE and OpenOCD.

Thanks & regards

=====================Debug log =========================================

Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:57)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 4000 kHz

adapter_nsrst_delay: 100

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 4000 kHz

Info : connected to stlink-server

Info : stlink-server API v1, version 1.3.0

Info : STLINK V2J36S7 (API v2) VID:PID 0483:3748

Info : using stlink api v2

Info : Target voltage: 3.180552

Info : SRST line asserted

Warn : UNEXPECTED idcode: 0x2ba01477

Error: expected 1 of 1: 0x1ba01477

Oct 17, 2019 2:27 PM UTC

Hi Paul,

I'm glad you find a way to use your dev board even if the device ID is not correct.

I would add that for test or learning purpose it is OKish to use the bluepill with the strange part as it is, but for anything that goes into production you should always use real product.

Best regards,

Kraal

S.Ma
Principal
Mar 17, 2020 5:29 PM UTC

Hmm the MSB bits of the ID Code register are just a version number so 2 means newer than 1.. ?

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.100230_0002_00_en/Chunk424975896.html

PGroe.2
Associate III
Sep 30, 2020 11:47 AM UTC

So you tweaked the config files for the openocd server, but what if I want to use the ST-Link GDB Server and not Openocd?

Tesla DeLorean
Guru
Sep 30, 2020 12:14 PM UTC

Might want to consider using authentic ST parts rather than GigaDevices clones.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PGroe.2
Associate III
Sep 30, 2020 1:14 PM UTC

Luckily I also ordered some replacement STM32F103 MCU's and soldered them onto the blue pill. They seem to have a correct vendor id and work with CubeIDE... ;).

PZwar
PZwarAuthor
Associate
Sep 30, 2020 12:01 PM UTC

I'm sorry, I do not have a solution for that.

Douglas MILLER
ST Employee
Dec 19, 2023 11:06 PM UTC

This forum thread was marked by the moderator as needing a little more investigation, so a Support case was created in your name and will be handled off-line.

Associate II
May 24, 2024 5:06 AM UTC

Info : STLINK V2J44M29 (API v2) VID:PID 0483:374B
Info : Target voltage: 3.189084
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : [STM32F103C8Tx.cpu] Cortex-M3 r2p0 processor detected
Info : [STM32F103C8Tx.cpu] target has 6 breakpoints, 4 watchpoints
Info : starting gdb server for STM32F103C8Tx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
[STM32F103C8Tx.cpu] halted due to debug-request, current mode: Handler HardFault
xPSR: 0x01000003 pc: 0xfffffffe msp: 0xffffffd8
Info : device id = 0x20030410
Info : flash size = 128 KiB
shutdown command invoked
Info : dropped 'gdb' connection

 

 

[STM32F103C8Tx.cpu] halted due to debug-request, current mode: Handler HardFault
xPSR: 0x01000003 pc: 0xfffffffe msp: 0xffffffd8

facing this error in

STM32F103C8T6 board

could not verify the st device