Hello techies,I am using STM32H563MI for one of the embedded application, I have to start the design hence looking for readily available OrCAD library.Appreciate if anyone has the library for schematic and Allegro layout footprint. This helps my tea...
I've checked the documentation tab on the product page and also in the user manual, but can not find it.Is it available somewhere?Thanks,josh
Hi,I purchased this STM32H723 mini core board that has 20 pin fpc connector for camera module and 10 pin fpc connector for LCD module.https://www.aliexpress.com/item/1005005852859518.html?spm=a2g0o.order_list.order_list_main.10.d0bd7385STni3J&gateway...
I desinged a custom board using STM32H743IIT6. But I can't Debug it.Reset is pulled highBoot0 is pulled lowVDD is stable at 3..28V at all desired pins of the boardVCAP 1&2 connected to 2.2uF capacitors...VDDA is 3.28V, VSSA is GroundedI tried manythi...
Hello Team,I encountered an issue while using the ST-LINK GDB server version 7.6.0. The server started successfully, but it failed when attempting to halt the target. Below are the server messages and the steps I’ve taken to troubleshoot the problem:...
Hi I am designing a PCB using STM32H563ZI. Can you share the project files for NUCLEO-H563ZI ? I am using Altium Designer. If the files are in different format, I can import them to Altium. I have shared the link and the name of the evaluation board ...
I have successfully implemented the USB_OTG_FS as host as mass storage class on the STM32F407 discovery board. Now I want to do the same with the USB_OTG_HS But there is no usb connector available on the discovery board Can anyone guide me what exter...
Hey everyone, I am working with the ADXL 354 eval board with an STM32H745data sheet ADXL354 : https://www.analog.com/media/en/technical-documentation/data-sheets/adxl354_adxl355.pdfdata sheet eval boad: https://www.analog.com/media/en/technical-docum...
I have tested the POC (Proof of Concept) by using 'Nucleo-439ZI' evaluation Board. I am now going to use the same schematics as reference for my prototype and create a custom board by removing the Morpho and Zio connectors as well as the unintended f...