STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F769I-EVAL SDRAM information

Hello,I'm working on the STM32F769I-EVAL.In the User Manual 2035, version 3 (last version), on the SDRAM schematic, the address pin are mapped such as:A0 to A11 are connectedA12 and A13 are not connectedA14 and A15 are connectedSo I have some questio...

ANauz.1 by Senior
  • 258 Views
  • 3 replies
  • 0 kudos

Resolved! Given the correct hardware configuration, is it possible to access two different external memory types (SRAM and Flash) by use of the same FSMC bus?

I have an application where it is necessary to read data from external flash to perform operations on data stored in external SRAM by using the same fmc connections. In this case the parallel interface is important as the operations are time sensitiv...