Resolved! STLink / STCubeProgrammer support on Windows ARM64
I can't get the STLink drivers installed on Windows 10 / 11 aarch64 Parallels VM running on Mac M1.Is there any support for ARM64 Windows STLink drivers?
I can't get the STLink drivers installed on Windows 10 / 11 aarch64 Parallels VM running on Mac M1.Is there any support for ARM64 Windows STLink drivers?
I am using STMCubeIDE v1.7 on MacOS 10.15.7 and connecting to my target via an STLINK V3. I updated CubeIDE to v1.7 and it suggested an update to the STLINK. Since doing that update I am not able to connect to my target (STM32F405). Errors given a...
Hi,I was trying to disable Tzen in my nucleo-l55ze-q (stm32l55), but before disabling i forgot to flash toggle gpio programmer into board, and tried to set RDP to 55 and i clicked apply,From that moment it is not able to detect the STlink!..please g...
Hello,I am using v2.2.0 over a ST-Link/V3 (FW version: V3J3M2B3S1).I connect to a STM32L471RGT6 MCU.Then I want to change the User Configuration OptionByte IWDG_STOP from 1 to 0.I get: Error: Option Byte Programming failed.Is this a bug or am I doing...
I am assuming this is a Windows driver issue, but I do not know how to resolve it. I use several Nucleo boards. Additionally, I use some USB ST-Link programmers.These programmers always show up with a single letter serial number: A, B,C, D.Using Kei...
My NUCLEO is powered by an external power supply of 5V on the E5V pin. The STLINK is detected on STM32CubeProg, but no board, no target voltage.. (Sometimes 0.01-0.03V)You could find below what I had already do for my installation.What did I do on th...
Hello there,I have just obtained the STLINK-V3 device:I have installed the STM32Cube Programmer (v 1.3.0) *** the drivers that comes along with it. The problem is that I cannot find the device:There is no drivers missing, the device manager is "clean...
I debuged my software on the STM32F722ZE, when I suddenly lost connection to it. I tried to connect to it with ST-Link V2 and Segger J-Link. Error message from J-Link commander is: Can not attach to CPU. Trying connect under reset. Connecting to CPU ...
On Windows 10, I just updated (again) to the 1.4.2 version, hoping to solve this issue, yet nothing changed.Already tried a clean install (again) and re-installed the latest STM32CubeProgrammer: nothing changed.Will ST handle this sooner or later ple...
Hello,I have been working with a Nucleo eval board and have not had any problems with the ST-Link connection. Recently I got an ST-Link/V2 ISOL dongle to use with a custom board using the same chip, and have been unable to connect with it. There seem...