B-U585I-IOT02A with external SD card
Hello forumI want to make a code that saves pictures from the camera module into an external SD card using SPII'm unsure what peripherals to activate and how to execute that, can someone help?thanks
Hello forumI want to make a code that saves pictures from the camera module into an external SD card using SPII'm unsure what peripherals to activate and how to execute that, can someone help?thanks
Hi,I'm willing to use the MXCHIP EMW3080B wireless module on the B-U585I-IOT02A in a project with TrustZone enabled. As there is no tutorial for that, I copied files from the Nx_Network_Basics example.Unfortunately I get the following error when buil...
Hi all I just designed my first custom PCB running on an STM32U585(VIT6). Or let's say it was desired to run on a STM32...As I couldn't get the MCU noticed by neither the STM32CubeMX nor the STM32CubeProgrammer, I designed another board that just h...
I'm using Nucleo-U545 for my project and set the external interrupt for user button as follow.void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin){if(GPIO_Pin == USER_BUTTON_Pin) { HAL_GPIO_TogglePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin); printf("*b...
Dear, I want to use SMPS of STM32 using this schematic Can you review this if i'm correct ? Thank you
I am planning to use an STM32U5 SPI peripheral and I want to do a SPI read of a "black box" that doesnt exist yet. currently the planned output of this device has this configuration where the chip select is high for 5 bytes of data. the STM32U5 is ca...
Hello forum,Im trying to build a function based on the BSP example and all the peripheral sensors,when opening a new project and adding the libraries and drivers from the BSP example, nothing works.some of the files have missing defines which suppose...
This is a switching regulator and they require the specified output capacitance which is 4.4uF given in the datasheet we have given two 2.2uF capacitance at the regulator but one capacitance has 2 ohms resistor to it for intrinsic safety will this st...
Hello,I'm programming an HSM following this video, but I don't fully understand how the HSM works.That is, once I program the HSM, what does it mean? What is "HSM version Maximum counter" and how does it work? How can I rerun the processes from the v...
Hi!Is there download link for the code in this demo. ?More specifically, I am interested in the code that generates the FPS and MCU load.Thanks in advance