STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F072 USB Connection

Hello everyone!I have a problem regarding my STM32F072 MCU board that I designed: I cannot connect the board with a terminal properly. Let me explain:1. I've managed the program the board using ST-LINK V2 (Chinese version) and SWD pins.2. When I conn...

AlexB99 by Associate II
  • 151 Views
  • 1 replies
  • 0 kudos

STM32F072B-EVAL SD card image

Hi,I am looking for a SD Card image from STM32F072B-EVAL kit. Without it demo program can not run. Package from ST site (en.stsw-stm32137) contains files from SD card, but it seems it does not work. I will be grateful for help.

pawelr by Associate
  • 116 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F030C6 breakpoint setting does NOT work on STM32CubeIDE using ST-link V2. Is it a BUG or setup issue? and how?

When I hit Debug. System stops at first line of main() as intended. However no matter how I setup any breakpoints on the rest code, and hit Resume(F8) button. The code never stops on those breakpoint. even though I am 100% sure those breakpointed li...

BLu.397 by Associate
  • 4600 Views
  • 10 replies
  • 5 kudos

Resolved! Can we set Boot0 in Software?

Hello,I am working on a project where we have a main board and a header board connected via SPI. We have the ability to update the firmware of the main board over the air but not for the header board. We now have a need to update the firmware of the ...

cluelezz_0-1713473044908.png
cluelezz by Associate II
  • 384 Views
  • 4 replies
  • 0 kudos

Nucleo-F072RB USB

Hello,I am having trouble getting the USB peripheral recognized by the PC device manager.  In Cube I have the USB FS device checked, and the USB_DEVICE middleware set to virtual COM port.  Everything else is set to default.The USB clock is set to 48M...

bwissel by Associate II
  • 750 Views
  • 16 replies
  • 2 kudos