DSI to HDMI adapter B-LCDAD-HDMI1
Quick question, maybe.Is there a cable assembly that can be recommended that will plug into CN1 (DSI Port) on the B-LCDAD-HDMI1 DSI-HDMI adapter? Thanks,TJM
Quick question, maybe.Is there a cable assembly that can be recommended that will plug into CN1 (DSI Port) on the B-LCDAD-HDMI1 DSI-HDMI adapter? Thanks,TJM
Hi everyone,I’m working on a project that requires developing a driver for the Goodix GT2931 capacitive touch controller using an STM32 microcontroller. While I’ve set up basic I2C communication in STM32CubeMX, I'm struggling with the driver code imp...
Hi, @Erwan SZYMANSKI @KDJEM.1 @Andrew Neil @KDJEM.1 @SofLit I am trying to establish SPI communication between my Nucleo-G431RB and STM32MP157F-DK2 boards. I am finding the documentation quite confusing. I attempted to use STM32CubeIDE, but it result...
Hello team,I’m working with an STM32H745iik6/ Nucleo-H745ziq microcontroller and currently using USB DFU mode to upload firmware. The process involves setting BOOT0 to 1 and performing a manual reset to enter DFU mode. After uploading the new firmwar...
I am currently Attempting to get Lorawan Fuota working for a duel core system. It is without question connected to my device and it seems to work fine. On the software end, attempting to use build.bat appears to work fine as well. But whenever I atte...
Hello team,I am working on a project involving an STM32 microcontroller, and I am looking for guidance on how to implement remote firmware updates. Specifically, I want to be able to update the code on the microcontroller over the air (OTA) without n...
Hello,I am new to the STM32 platform and will be using it to prototype an embedded controller. I ordered an STM32H7S78-DK Discovery board since it had all the necessary IOs available and included a touchscreen display. However, I also need Bluetoot...
Can I safely get that power out of any of the nucleo PD boards with a usb3 pd input? Can I get any higher current or voltage? Output is 2 pin barrel connector. Target application is fully documented here. Thanks so much in advance Joe
is there anyone who worked with the MB1400 Wi‑Fi module or has an idea about it? I'm working with the STM32H7 Nucleo-144 board and I need to add a Wifi module, I find a problem when connecting the module to the card I can't understand how to match th...
Hi,I purchased this STM32H723 mini core board that has 20 pin fpc connector for camera module and 10 pin fpc connector for LCD module.https://www.aliexpress.com/item/1005005852859518.html?spm=a2g0o.order_list.order_list_main.10.d0bd7385STni3J&gateway...