STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI SD Card Library

Hi,I followed this tutorial to have made FatFs library work on my STM32 F411 PCB board with SPI interface.Basically I need to store 1000+ floating point values in SD card and read them back.I have no problem in writing; but I cannot read all the reco...

HDaji.1 by Senior
  • 944 Views
  • 0 replies
  • 0 kudos

Doubts on Nucleo-H753ZI

I'm interfacing Nucleo-H753ZI with DAC8775EVM through SPI4. DAC8775EVM works on logic HI in range of 5V and expects the same logic from Nucleo-H753ZIbut Nucleo-H753ZI MCU itself runs at 3.6V so Logic Hi isn't read by DAC8775EVM.How to Change the logi...

Stm32 pcb on spi wifi soc?

Hello everyone. What do you use as wifi module or ic in your pcb circuits, including stm32 processors. I don't like working with AT commands. I would like to work with SPI or SDIO interface if possible. Can you suggest a solution with libraries and s...

mcizmeci by Associate II
  • 355 Views
  • 0 replies
  • 0 kudos