Skip to main content
c_dev05
Associate II
Oct 18, 2019 7:30 AM UTC
Question

Option Bytes programming not working

Hello,

I am using v2.2.0 over a ST-Link/V3 (FW version: V3J3M2B3S1).

I connect to a STM32L471RGT6 MCU.

Then I want to change the User Configuration OptionByte IWDG_STOP from 1 to 0.

I get: Error: Option Byte Programming failed.

Is this a bug or am I doing something wrong?

Log:

09:29:04 : Option byte command : -ob IWDG_STOP=0 

09:29:04 : PROGRAMMING OPTION BYTES AREA ...

09:29:04 : Bank : 0x00

09:29:04 : Address : 0x40022020

09:29:04 : Size : 20 Bytes

09:29:04 : Reconnecting...

09:29:05 : Reconnected !

09:29:05 : UPLOADING OPTION BYTES DATA ...

09:29:05 : Bank : 0x00

09:29:05 : Address : 0x40022020

09:29:05 : Size : 20 Bytes

09:29:05 : Bank : 0x01

09:29:05 : Address : 0x40022044

09:29:05 : Size : 16 Bytes

09:29:05 : OPTION BYTE PROGRAMMING VERIFICATION:

09:29:05 : Error: Expected value for Option Byte "IWDG_STOP": 0x0, found: 0x1

09:29:05 : Error: Option Byte Programming failed

This topic has been closed for replies.

5 replies

Houda GHABRI
ST Employee
Oct 23, 2019 10:16 AM UTC

Hi @c_dev05​ ,

Thanks for your feedback.

This problem will be fixed soon ,in the meantime you can unplug/plug the board after modification of OptionByte  and will be Ok.

Regards,

Houda

c_dev05
c_dev05Author
Associate II
Oct 23, 2019 11:56 AM UTC
Hello,
I implemented option modification also into my firmware, that is running on the STM32L4 MCU.
And I am also seeing strange behavior:
* I change the option byte; read it back and it still has the same value.
* I make a reset and it still has the old value
* I un-power the MCU; wait a few seconds and power again => option byte has new modified value.
Please can you tell me how you fix this problem in the programmer? I want to do the same in my code.
regards,
toroid
Explorer II
Feb 3, 2021 12:08 PM UTC

I experienced same issue with STM32F427. My board was bricked because of this but I did manage to find a way to revive it again.

So problem began when I tried to set option bytes from code, something went wrong, and all option bytes were set and none could be removed. I got the same error, doesn't matter if I disconnect/connect/power cycle. Read protect (RDP) is 0xAA.

3:50:52 : Option byte command : -ob nWRP0=0

 13:50:52 : PROGRAMMING OPTION BYTES AREA ...

 13:50:52 :  Bank         : 0x00

 13:50:52 :  Address      : 0x40023c14

 13:50:52 :  Size         : 8 Bytes

 13:50:52 : UPLOADING OPTION BYTES DATA ...

 13:50:52 :  Bank         : 0x00

 13:50:52 :  Address      : 0x40023c14

 13:50:52 :  Size         : 8 Bytes

 13:50:52 : OPTION BYTE PROGRAMMING VERIFICATION:

 13:50:52 : Error: Expected value for Option Byte "nWRP0": 0x0, found: 0x1

 13:50:52 : Error: Option Byte Programming failed

Strangely, I tried using the UART bootloader (stm32flash or STM32CubeProgrammer v2.6.0 command line) and it appear to be able to remove write protection and program the MCU, but in reality it does not and problem remains.

However, adding read protection was possible through STM32CubeProgrammer GUI. I connected by SWD to the MCU and set read protection to level 1. Point of this is that this should cause an MCU internal flash erase operation (does not need debugger) if a read operation is attempted. Now how to trigger that, I found that if I connect by STM32CubeProgrammer GUI in UART mode (see picture below), it gives the option of 'read unprotect (MCU)' which triggers the flash erase operation. This actually fixed my issue and my MCU is alive again.

UPDATE:

It is possible to do this without the UART bootloader in command line with these commands:

STM32_Programmer.sh -c port=swd --optionbytes RDP=0xBB (to enable read out protection)

STM32_Programmer.sh -c port=swd -rdu (to trigger mass erase)

The 'read unprotect' option is available also in DFU mode (at least).0693W000007Dm1GQAS.png

Explorer
Dec 16, 2023 3:57 PM UTC

You saved me

Tom MacDonald
Associate III
Oct 6, 2021 2:53 AM UTC

Thanks for your post, this helped me undo write protections that I had set on my MCU.

In my case, there was no need to use your "connect under UART" step --> all I needed to do was toggle RDP to level 1, change WRP bits, then toggle RDP back to level 0 to get back to normal.

Still, WTF?

 0693W00000FBZbdQAH.png