I can't get the STLink drivers installed on Windows 10 / 11 aarch64 Parallels VM running on Mac M1.Is there any support for ARM64 Windows STLink drivers?
I was able to make this work end to end with STM32CubeProgrammer and IAR on Windows 11 ARM64 (running in Parallels on an Apple M1). To make that work, I have removed all references to the certificate signatures (CAT files) from INF files.To install, ...
Just an observation (completely different from the original problem): I've diffed yours and mine and found two devices appear only in the x86 section but not in the amd64 (so because I've duplicated the amd64 one, I have not included them). ST should...
Sure! Again, Pavel's solution is really something that must be done by ST and cannot be worked-around by the community. The changes I've made cannot work (for security reasons as the driver package is signed). The changes are following driver documen...