STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C HAL_BUSY NUCLEO-FR103RB Master

NUCLEO STM32 I2CHello, I'm trying to make a master NUCLEO-FR103RB send data to a slave device using fast mode (400 kHz). Slave to master is not essential at the moment. As slave I am using the Total Phase AARDVARK in slave mode simulating a LED drive...

image_2024-09-19_131011655.png I2C.drawio (1).png
xenon by Associate
  • 168 Views
  • 6 replies
  • 3 kudos

Do STLINK-V3 have a power output?

I have a STLINK-V3SET and I'm trying to comunicate with a STM32F103C8T6 (Blue Pill). I'm sucessful only when the board is externally powered by it's USB port. The STLINK-V3SET SWD or JTAG connectors have a T_VCC pin, which I now realized are an input...

roitav_1-1724329721339.png roitav_2-1724329831411.png roitav_0-1724329522418.png
roitav by Associate
  • 263 Views
  • 3 replies
  • 2 kudos

STM32F103C8T6 Blue Pill project

First and foremost, as of this point I know virtually nothing about these MC's but through this project, I'm hoping to learn. What I'd like to get some assistance on is just a few basic pointers and perhaps direction so that I'm not chasing my tail.T...

jw11432 by Associate
  • 286 Views
  • 2 replies
  • 1 kudos