STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1383 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 546 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to clone/copy an STMCube Example project

Hello,I'm new to STM32Cube-IDE (and Eclipse). Normally I use the ARM-gcc toolchain and do assembly coding.I managed to create a New STM Project by using the Example Selector tab in the Target Selection window.In this case it was the BSP Example for t...

Screenshot 2024-08-11 at 02.02.14.png
cc2 by Associate
  • 2701 Views
  • 3 replies
  • 1 kudos

Live Expressions showing wrong values

I am using CubeIDE version 1.11.0 for a STM32F411RC project. After i've changed boards (between two equal custom boards), my live expressions started showing wrong values. The values are only wrong in the live expression, because if I halt the progra...

THML by Associate II
  • 6512 Views
  • 9 replies
  • 5 kudos

Resolved! Unable to install STM32CubeIDE plugin from jar file

I bought an analysis program from a company and they gave me a plugin .jar file to install the analysis program in IDEs. When I put this plugin .jar file in a folder called dropins in the Code Composer Studio IDE folder, it works directly. But in STM...

dikene by Associate II
  • 1039 Views
  • 1 replies
  • 0 kudos

Resolved! Comments folding issue

Hello all, i have reported it several times but ST has successfully ignored it. So i am posting it here. In CubeIDE is folding not working if file is long (around 3k lines). This is a major problem because a lot of LL "drivers" (BTW, it is RAL-Regist...

Eiffel by Senior
  • 1438 Views
  • 3 replies
  • 5 kudos

Resolved! SFRs are not shown in the STM32CubeIDE in Debug mode

Hello,STM32F411CE microcontroller.I created a starter project via STM32CubeMX using HAL and opened it in STM32CubeIDE. When I run this project in debug mode, the SFRs tab is empty (see figure bellow). Why?When I create a project without using STM32Cu...

Mykola_Levun_0-1750324035376.png

issue in opening two file in fatfs stmcube

Hello,I have been trying to open two files simultaneously in sdcard (one in READ mode and another one in Write mode) using the STMCUBE IDE fatfs library. Since two files requires two file handles so I have defined below mentioned parameters in the fa...

shefu_0-1715236162842.png
shefu by Associate II
  • 2925 Views
  • 4 replies
  • 0 kudos