STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1280 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 513 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! With the ADC using single ended input channel, what is the internal vref, what is the 12 bit voltage range for measurement (is it 0 to 2.5V or 0 to 3.3V)? What is the lowest accurate measurement resolution when we have less than 20mV to measure?

I am trying to work with photo diodes and need to measure 20mV or less with ADC. Whats the best resolution I can get with a single ended ADC (using ADC 3 channel 12 at the moment).Whats the measurement range on that channel? When we have less than 10...

PRedd.111 by Associate III
  • 1542 Views
  • 2 replies
  • 0 kudos

How to perform Firmware Upgrade on STM32F413 Discovery Board.

Hi, We are looking to perform a firmware upgrade on STM32F413 where the firmware upgrade image is coming over BLE chip which is interfaced over UART to this controller. Can I know if any procedure was available to perform this operationRegardsSrikan...

Smedi by Associate II
  • 925 Views
  • 1 replies
  • 0 kudos

Question about redefinition

Hi all,just a short question:Why does the compiler say that the page is redefined?#define ADDR_FLASH_PAGE_148 ((uint32_t)0x0804A000) #define ADDR_FLASH_PAGE_149 ((uint32_t)0x0804A800)Same page but with small letters and that's ok for the compiler...

eschl by Associate
  • 2566 Views
  • 4 replies
  • 0 kudos

Open in new window => STM32CubeMX view get's corrupted

Hi,I'm working with multiple monitors. I had to compare two STM32CubeMX files from two projects in the project tree. So, I right-clicked on one project, selected 'open in new window', and then openend the corresponding STM32CubeMX file. Both views of...

RAltm by Senior
  • 938 Views
  • 0 replies
  • 0 kudos

Problems debugging from STM32CubeIDE and Linux Debian

Hello developers,I am a beginner in STM32 programming.I have the board STM32L152C-Discovery, the ST-Link V2 adapter and Linux Debian on my laptop installed.I am using STM32CubeIDE as IDE.I setup my first project in STM32CubeIDE with the automated cod...

MHof by Associate II
  • 7181 Views
  • 8 replies
  • 0 kudos

CubeF0: LL_DAC_init does not set DAC trigger source

Using STM32IDE LowLayer and STM32F051C8This code does not set the triggersource for the DACDAC_InitStruct.TriggerSource = LL_DAC_TRIG_EXT_TIM15_TRGO; DAC_InitStruct.OutputBuffer = LL_DAC_OUTPUT_BUFFER_ENABLE; LL_DAC_Init(DAC, LL_DAC_CHANNEL_1, &DAC_I...

Willunen by Associate III
  • 917 Views
  • 0 replies
  • 0 kudos