STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1281 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 513 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hi, acquiring analogue signal, using STM32 F3 DISCOVERY, I'd like to be able to read the values on the screen through TERA TERM, but I can't activate the serial port. Can you tell me what the problem is please?

Hi, Through STM32CubeIDE I'm acquiring analogue signal, using STM32 F3 DISCOVERY.The converted values ​​are saved in a register, then I'd like to be able to read them on the screen through TERA TERM, but I can't activate the serial port. Can you tell...

IValo by Associate
  • 1210 Views
  • 2 replies
  • 0 kudos

Resolved! Not receiving DMA Transfer Complete interrupt.

I'm using both SPI1 and SPI2 on an STM32G071RBT Nucleo board, using STM32CubeIDE code generation and LL interface. Both SPIs are configured to use DMA for receive and transmit. SPI1 uses channels 2 & 3; SPI2 uses channels 4 & 5. The DMA transmit co...

BCoch by Senior
  • 4436 Views
  • 3 replies
  • 0 kudos

Breakpoint based on memory written

I am debugging with STM32CubeIDE, and I have a problem in my program of something unrecognized writing in the memory space. To be more specific in the 0x20001FBCCould it be possible to define a breakpoint in the debugger that shoots when this memory ...

Eclipse Color Themes extension

Hi! So, TrueSTUDIO supports the Eclipse Color Theme extension right out of the box.STM32CubeIDE instead does not, but not only: even after searching for it in the Marketplace, it does not show up. Why?I know that maybe this is not an high priority is...

Lori B. by Associate III
  • 1903 Views
  • 1 replies
  • 1 kudos

Multiple MCU support in a static library project

Some time ago I created a static library project in AC6 System Workbench for STM32. The project expanded and I started to adding build targets for more microcontrollers, STM32L, STM32F7, etc. After migrating the project to Cube IDE I am no longer abl...

0690X000009k2OhQAI.png
MMatu by Associate III
  • 942 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE on MAC Mojave and .dylib ... Resolved!

When I started a debug-session, I got the following message:dyld: Library not loaded: /opt/local/lib/libusb-1.0.0.dylib Referenced from: /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server....