STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1381 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 545 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Unable to read STM32CubeIDE repository

Hi guys! I need to solve this:Unable to read repository at http://sw-center.st.com/stm32cubeide/updatesite1.Unable to connect to repository http://sw-center.st.com/stm32cubeide/updatesite1/1.0.1/content.xmlConnection refused: connect

BAkar.1 by Associate
  • 1693 Views
  • 1 replies
  • 0 kudos

Resolved! how to use float in printf?

Float in printf doesn't seem to work in new projects created in stm32cubeideIf i create a project in sw4stm32 it works, there, it also works if i import the sw4stm32 project, it does not work if i create a new project in cubeideIn all cases the opti...

Simple HelloWorld ANSI C Project with STM32CubeIDE ?

I'm preparing a basic embedded programming course. I will use some Nucleo boards with CubeIDE. For the bases of C and C++ programming, I also want to use CubeIDE but I didn't found the documentation for configuring STM32CubeIDE to compile a simple AN...

BTrem by Associate II
  • 7587 Views
  • 6 replies
  • 0 kudos

Resolved! Problem on I2S output using HAL

Hi,​I wrote a simplest program (below) to send sine wave data to PCM5102A (DAC) via I2S.​However, I found only L-ch data is valid and R-ch has no data.Analogue (DAC) output of L-ch is somewhat sine wave, but it is sometimes de-formed. And if I look i...

0693W000000XN2BQAW.png
KAJIK.1 by Associate III
  • 5796 Views
  • 5 replies
  • 0 kudos

Resolved! installation of the stm32cubeide

i have got a problem when i download stm32cubeide and install. i have download the file "en.gnu-tools-for-stm32-7-2018-q2-update.20190328-1800.zip" is correct? i have extracted the file, but can not find out the installation file in extract folder. ...

kevin xu by Associate II
  • 2054 Views
  • 3 replies
  • 0 kudos

Wrong download link for STM32CubeIDE

Tried downloading STM32CubeIDE for macOS and Linux (Debian installer). Both of these are not giving the correct download file. It seems to be some kind of source code package to compile a toolchain. Please help!