Hi,The link of latest version of STM32CubeIDE is broken. When I try to download the v1.3.0, the download system redirect gnu-tools-for-stm32 instead of cubeide.Regards,Ibrahim
Hi,I'm trying to get PTP timestamp on STM32H743 Nucleo board. There is no proble with LwIP and ethernet driver so far except for PTP. I followed the instruction( 58.9.7 Programming guidelines for IEEE 1588 timestamping) on reference manual (RM0433) a...
Hi,We are trying to develop a pedometer based on LIS3DSH. We already have aSTM32F4 (F407) discovery board equipped with LIS3DSH. As stated in the document"Application Guidelines for LIS3DSH State Machine", there is anapplication "Pedometer Based on S...
Hi @TwelveSquared and @Community member I'm able to download v1.2.0 from dropdown menu on the download page and updated to v1.3.1 within STM32CubeIDE.Hope that helps.
The problem comes from the Sub-second increment register (ETH_MACSSIR). The value to be incremented is stored in high word of the register as in the image below.Everything runs as expected when changed the value as follow.WRITE_REG(heth->Instance->MA...