STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1420 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to uninstall STM32CubeIDE

Hello.I use Debian Buster an I downloaded STM32Cube IDE from here:https://www.st.com/en/development-tools/stm32cubeide.htmlI used the Linux debian package (.deb file) and ran the sh script that comes inside the zip file (version 1.3.0).Since this is ...

May had a bug in STM32CubeIDE V1.4.0

I recently upgraded STM32CubeIDE to version 1.4.0 and opened a previous project in it. After opening the .ioc-File from the project, I noticed that the NVIC-settings had all changed.The settings were correct when I opened this .ioc file with CubeMx v...

Slh by Senior
  • 554 Views
  • 0 replies
  • 0 kudos

Using firmware examples

Hi to all!There is a way for using the firmware examples without broke nothing?I want to use and modify some examples, but it's not seem an easy task..If I use "import existing project into workspace", if i use copy project into workspace, the impo...

Luca1 by Senior
  • 4253 Views
  • 9 replies
  • 0 kudos

Resolved! How to run without debug

Trying out the new STM32CubeIDE. Mostly, I like it. There are some rough edges and dialogues that do not behave properly (at least on the Mac) but the thing I cannot make work is to add a 'Run' configuration to the toolbar.I want to just build the co...

Hi! I am new to all this stuff. While transfering Keil project to Cube IDE I'm facing many issues, is there a proper step by step tutorial or help on how to transfer kei project to cubeIDE? Also help me with following errors

Errorsfatal error: rt_sys.h: No such file or directory #include <rt_sys.h>I have this fuction in somefile  __asm void MSR_MSP(u32 addr){  MSR MSP, r0 //set Main Stack value  BX r14}error: expected '(' before 'void' __asm void MSR_MSP(u32 addr)error...

AKhan.6 by Associate
  • 1416 Views
  • 4 replies
  • 0 kudos

STM32G070: UART speed of 115200 is not possible with PC when running SYSCLK clock at 64MHZ - however is when run at 59.0MHZ

8MHZ HSE crystal. HSE selected and PLLCLK selected.64MHZ / 115200 / 16 = 34.7222Assuming the CPU picked 34 as the divisor then the baud rate is 117647.1 2% too highBut setting to 59MHz I was able to successfully communicated at 921,60059MHZ / 921600 ...

0693W000003BZ39QAG.png