STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1417 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE C++ Generation and Language Mapping

Hello Everyone,I am having some trouble getting the STM32CubeIDE to work with C++ on my STM32F4 Project.I have converted my project to a C++ project and Renamed source files withing the IDE.This works ok and compiles fine. with g++ being used to comp...

0693W000003BeD4QAK.png 0693W000003BeEHQA0.png
TCash.1 by Associate III
  • 3429 Views
  • 1 replies
  • 0 kudos

Resolved! How to obtain the dwarf2 file to simulate with proteus isis

Hi all, I'm trying to simulate a project for an STM32F103C6 in proteus ISIS but for debug purposes labcenter's people says that I need the .elf file and the dwarf2 file (both of them in the same folder), then I' found that GCC generates the dwarf 2 f...

VRami.1 by Associate III
  • 5115 Views
  • 3 replies
  • 1 kudos

Resolved! I cannot use the HAL functions for ADC?

Hey there,I tried to modify an existing project by using the ADC to measure a current. My problem is when I try to include the header stm32l4xx_hal_adc.h and use the functions like HAL_ADC_Start(); i will get the error undefined "reference to...". I...

0693W000003BaB4QAK.jpg
SStad.1 by Associate II
  • 8047 Views
  • 24 replies
  • 0 kudos

Using a TIM2 for µs measurement in thread in combination with FreeRTOS leads to HardFault_Handler being called.

I'm working with the Nucleo-G474RE Board. With the STM32CubeIDE I set up FreeRTOS and assign TIM6 as Timebase Source (as recomended by the IDE). I create a basic Thread to test a basic scoped timer I want to use for timing measurement. The ScopedTime...

0693W000003BaODQA0.png 0693W000003BaeBQAS.png
JHöfl.1 by Associate III
  • 1179 Views
  • 1 replies
  • 0 kudos

QUAD SPI read not working

Hi all,I am working with STM32L476RG and using ST32cubeIDE for developing project. I am trying to enable Quad SPI in my project . I am using MX25R8035FM1IL0 as flash memory. I followed the code in the software package of ST, but it is not working. Wh...