STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32 OTA? Goodbye to ST-Link? How to upload via internet?

I found a project that allows the programming of STM32 via OTA, it would be very interesting if the STM32CubeIDE could work directly with this.[STM32 OTA using esp8266]:https://www.youtube.com/watch?v=aqYHebO789UDoes anyone know if it is possible to ...

by Not applicable
  • 2172 Views
  • 2 replies
  • 1 kudos

Resolved! In STM32CubeIDE, can I add python script to auto-run before compiler runs? To increment a BUILD number in *.H file.

In old AC6 workbench, I could add such python script as external tool to auto-build always before compiler runs. Now with STM32CubeIDE, I've found how to do manually with 'external tools' button. Can I add back to project to auto-run again?

Resolved! edit makefile

HelloI am using stm32Cube IDE.Where should I edit the makefile?Thank you.

Ebun.1 by Senior
  • 3483 Views
  • 2 replies
  • 0 kudos

Can't include new folders in STM23CubeIDE project?

I've created a new folder inside the User directory where main.c is, but when adding the path in the includes list it still can't find it?I've done it exactly the same way as the other two but for some reason it's just not working now.If I move the f...

JWood by Associate II
  • 2406 Views
  • 3 replies
  • 0 kudos

Ask for errors related to 'Mon64.dll'

Hello, colleaguesI have a problem in building the project.I installed STM32CubeIDE (Ver. 1.4.2) and generated code successfully.(I applied only the clock configuration and RCC setup)When I tried to build the project, however, I faced several errors l...

0693W000003Pi28QAC.jpg
HKim.9 by Associate
  • 960 Views
  • 0 replies
  • 0 kudos