STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1403 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Best way to duplicate a workspace with projects

Hi,Let's say I have a workspace with multiple projects (e.g. application project, bootloader project, etc.) for a product. Let's say this workspace is located in C:\ProductA. Now I would like to duplicate this workspace to use it for another product ...

Anguel by Senior
  • 8416 Views
  • 9 replies
  • 3 kudos

Resolved! How to enable compiler/linker to manage external memory?

I've managed to get the SDRAM up and running on my STM32H745 Disco board. I've confirmed this by usinguint32_t* sdram = (uint32_t*) 0xD0000000; sdram[0] = 0xDEADBEEF;and checking the memory content. However, doing it this way, I have to control the a...

0693W00000BaAfeQAF.png
Hansel by Senior
  • 4764 Views
  • 4 replies
  • 3 kudos

Resolved! Wrong version number of CubeIde shown

I have CubeIde 1.61 installed on Win10/64 hard disk. About box/dialog says it is version 1.61, that is, the current version. Desktop icon or shortcut says it is version 1.40 or something. That is the original version number I installed sometime ago a...

LMI2 by Lead
  • 1992 Views
  • 4 replies
  • 1 kudos

Resolved! How to merge two CubeIDE example projects into one?

STM32H735G-DK has a number of projects as deliverables examples(ADC, LED,DMA,RTC,...).Are there some rules or tutorials for join two projects as single one project?(From two main.c => one single main .c and what else should have to do ?) in StmCubeID...

Ncons.1 by Associate
  • 1361 Views
  • 2 replies
  • 0 kudos

Resolved! Disable interrupts while Stepping Debug

I use to develop with IAR.I try to go to STM32CubeIDE.I cannot find the way to stepping debug a program if an interrupt timer is running in background.Is there an option like IAR "disable interrupts when stepping"Thanks

COSEBE by Senior
  • 7060 Views
  • 6 replies
  • 0 kudos

�?STM32F446(WLCSP81)】 How can I implement DMA for UART5.

I have an application for STM32F446.And I want to use DMA for UART5.But I can't set DMA for UART5 on STM32Cube IDE.Specifically I would set it on Device Configuration Tool And I would set DMA Request for UART5.But ​There is no choice for UART5 on DMA...

SNaga.4 by Associate
  • 1228 Views
  • 1 replies
  • 0 kudos