STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1436 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Doxygen with STM32CubeIDE

HelloI tried to use doxygen to a project folder from STM32CudeIDE but it does not generate the documentation. I also looked on how to use doxygen on eclipse but still no results.Is there a way to use doxygen or any other tool for generating documenta...

Avgerinos by Associate III
  • 5427 Views
  • 2 replies
  • 0 kudos

en.stm32cubeh7_v1-9-0\STM32Cube_FW_H7_V1.9.0\Projects\STM32H735G-DK\Demonstrations\Oscilloscope_SignalsGenerator\STM32CubeIDE

Oscilloscope_SignalsGenerator example Not Loading the Kit. i got the Error like Error in final launch sequence:Failed to execute MI command:load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscillos...

senthil by Associate II
  • 6293 Views
  • 13 replies
  • 0 kudos

Resolved! Missing IRQ Handlers in .s file

Hey, I'm having issues with my Nucleo Board.I'm using an STM32F410RB Nucleo board. I started a new project as usual. When I go to the reference manual and to the interrupt vector table, I see that the USART 1 and USART 2 are on positions 37 and 38, r...

Drexter by Associate II
  • 9918 Views
  • 11 replies
  • 0 kudos

Resolved! How to configure external eclipse stm32 project so that it can be debugged as cube cortex application

Our project firmware is build using cmake. Cmake is used to create Eclipse project like thiscmake ..\Firmware -G"Eclipse CDT4 - Ninja" -DCMAKE_ECLIPSE_VERSION=4.16I can import project to CubeIde without proplems and buid it there. Proplem is that Cub...

0693W00000BaAcuQAF.jpg
CEkho.1 by Associate II
  • 8884 Views
  • 12 replies
  • 2 kudos

Resolved! How can i use Build variables? pre-build shell script

I want the IDE to save inside a buildinfo.h various const strings containing build timestamp names and other system variables.But im unable to use them inside my pre-build script:#!/bin/sh echo "this is the pre-build script!:D"   set _current_date=${...

0693W00000BaHb5QAF.png 0693W00000BaHcwQAF.png 0693W00000BaHccQAF.png
Javier1 by Principal
  • 2920 Views
  • 3 replies
  • 0 kudos

Resolved! printf and scanf functions is not working in stm cube IDE

Hai,I am using the printf and scan f functions in my code of stm cube IDE, when I want to print some messages on VIRTUAL COM port , but the messages are not showing in my serial monitor. I dont know why it is not working , is there we have to write a...

RKUMA.2 by Associate II
  • 2828 Views
  • 3 replies
  • 0 kudos