STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1441 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to set up a breakpoint monitoring an address?

Hey all,I'm trying to verify register values in my project, as per this link: https://www.freertos.org/Debugging-Hard-Faults-On-Cortex-M-Microcontrollers.htmlI'm attempting to open the break point window in the debugger, and manually define an execut...

QHa.1 by Associate
  • 6042 Views
  • 2 replies
  • 1 kudos

Resolved! Is there a way to setup configMAX_SYSCALL_INTERRUPT_PRIORITY in freeRTOS on a STM32G0 ? It seems that this config is not available in STM32Cube Environnement and in freeRTOS port code

I am starting a new project on STM32G070KB and I want to use freeRTOS.Problem that I have is that the configMAX_SYSCALL_INTERRUPT_PRIORITY seems to be gone from the port !I use the latest STM32CubeIDE with the 1.4.1 firmware package for STM32G070KBPr...

WGend.15 by Associate III
  • 3814 Views
  • 3 replies
  • 1 kudos

Resolved! STM32CubeIDE 1.6.1 inactive code bug

Not sure where to report this.I have recently upgraded to OSX Big Sur and also to STM32CubeIDE 1.6.1Not sure when this issue started, I'm pretty sure it wasn't a problem before, and it does NOT happen on my Eclipse 2020-06 installation.Restarted, reb...

JHans.6 by Associate II
  • 5363 Views
  • 6 replies
  • 0 kudos

Code changes not being used in debug mode

Hi all, I am very new to this software so hopefully this is a silly question that is easily answered.I keep running into an issue where I can make a change in the editor, build the project and then look at the code step by step in debug mode, however...

0693W00000BcOAAQA3.png
RMyer.1 by Associate III
  • 1945 Views
  • 4 replies
  • 0 kudos

Freezing of stm32cubeIDE 1.5.1 on Ubuntu 18.04

Hello Dear, I have downloaded stm32cubeIDE 1.5.1 and install it. Troubles come when I launch the apps, it started and completely freezes and I could do anything before it shutdowns. Here the error messages that I get. Any suggestion? 

0693W00000BcFxrQAF.png 0693W00000BcFxhQAF.png
LBadi.1 by Associate II
  • 1384 Views
  • 2 replies
  • 1 kudos

Does STLINK allow debugging with breakpoints?

I am using a Nucleo-64 with the STM32F070RB on it with the STM32CubeIDE and I can flash my code to the memory but all I can do in debug is halting the CPU and reading out the registers. No user variables are allowed to be tracked and no breakpoints ...

MPers.1 by Associate II
  • 2076 Views
  • 5 replies
  • 0 kudos