cancel
Showing results for 
Search instead for 
Did you mean: 

hello does anyone know, if stm32cubeide works on the new mac m1? thanks

NTaha.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Julien D
ST Employee

Hi NTaha.1,

You can easily imagine that we can't commit on any milestones, anyway the community has to be aware of the existence of an internal initiative to support setups based Apple M1. Or well, first to provide a more precise answer :)

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

thanks, i'll waite :beaming_face_with_smiling_eyes:

Cartu38 OpenDev
Lead III

Eclipse first ... STM32CubeIDE then I guess ...

https://bugs.eclipse.org/bugs/show_bug.cgi?id=565690

ABrun.5
Associate II

Yes, it works fine, using Rosetta. I tested version 1.5 and board Discovery STM32F411

CSapa.1
Associate

Hi ABrun,

Good to know that it is working for you.

Any pre-requisite I need to take care for it to work? Xcode etc.

Am using M1 Mac Mini.

Thanks for the info.

Hello,

It worked immediately out of the box, I was surprised. It was one of the first programs that I installed. I don't have xcode yet, so I don't think you need anything else. To say the truth, most of the software I use works pretty well in the M1.