STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to add the CMSIS WiFi drivers to a STM32CubeIDE project?

I need to add support on a STM32 MCU to a WizFi360 WiFi module and noticed it is supported by CMSIS (https://arm-software.github.io/CMSIS-Driver/General/html/index.html), is there a specific way to add these CMSIS wifi drivers to an existing STM32Cub...

FGome by Associate II
  • 2259 Views
  • 2 replies
  • 0 kudos

Why is my #ifdef not working correctly?

I have a __BOOTLOADER symbol defined for my project as shown in the attached image I want to display firmware version based on the defined symbol so I have an #ifdef statement to select the correct string. The IDE displays the source code correctly:...

0693W00000CzdxqQAB.jpg 0693W00000Czdy5QAB.jpg
gsieb.1 by Associate II
  • 9291 Views
  • 7 replies
  • 0 kudos

PDM2PCM library

Hi, I am planning to convert PDM samples received from MP34DT05TR-A to PCM samples with 24 bit resolution at 48KHz sampling frequency using PDM2PCM library in stm32f401RE MCU. As per document PDM2PCM library only gives samples with 16 bit resoluti...

KK Y.1 by Associate II
  • 879 Views
  • 0 replies
  • 0 kudos

Is there any documentation on how to compile and flash the STM32CubeG0 MCU Firmware Package examples in STM32CubeIDE?

I haven't figured out how to get it to import an example in STM32CubeIDE and compile it. I tried to recreate the project based on one generated with STM32CubeMX, but had no luck.I eventually tried SW4STM32 and at least got it to compile there, but th...

LBode.1 by Associate II
  • 4155 Views
  • 7 replies
  • 0 kudos

Can't build a project after importing it

Here's the scenario:I have clean workspace. I have two projects on disk I want to import into the workspace. I store them on my Google Drive locally sync'd to my computer (Windows 10).I import one of the projects and try to build it. I can't beca...

Resolved! [SOLVED] Weird behavior debugging STM32H753

Dear experts,I hit a strange problem when debugging in CubeIDE code with a bootloader on Nucleo STM32H753.The bootloader sits in sector 14. The boot address of STM32H7 is redirected there via the option bytes. The main code starts at sector 0 (a.k.a....

Pavel A. by Super User
  • 1488 Views
  • 2 replies
  • 0 kudos