STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

how to use FPU in STM32F407

I am using STM32F407 discovery board which is ARM cortex M-4 based , which comes with FPU.I need to perform some Floating point number and exponent calculations. for that i need to use to FPU to speed up the process.I have have written all the perip...

Chopra.1 by Associate II
  • 16190 Views
  • 5 replies
  • 0 kudos

How explain debug data in STM32CubeIDE?

Hi! I am start work with STM32CubeIDE last time and I did not understand:Whay not work elementary function "HAL_GPIO_ReadPin"? Alwais retun "0" but pin state pfisicaly change and change IDR of PORT?Whay in Stop debug mode I see different data in reg...

0693W00000DmcOJQAZ.jpg
Pavel_MN by Associate
  • 1669 Views
  • 2 replies
  • 0 kudos

Firmware upgrade through Y modem

Hi , i am new to some of the peripherals of STM32 controllers...I am using STM32L151RCT6 MCU in STMCube IDE for my application..My requirement is like i need to receive the new firmware binary file via Y modem and need to write into the flash and nee...

MBhir.11 by Associate III
  • 9475 Views
  • 7 replies
  • 0 kudos

Problem occured on debugger : Error message from debugger back end: /usr/bin/arm-none-eabi-gdb: Error in sourced command file

Hello,i work on Archlinux, and i recently installed STM32CubeIDE. I previously had some issues with arm-none-eabi-gdb, which couldn't check the version because of the missing library libncurses5 (which was on version 6 on my computer). So i downloade...

ASEGU.1 by Associate II
  • 917 Views
  • 0 replies
  • 0 kudos

FLASH MEMORY FULL

I am using STM32L011K4 with 16KB flash memory. I did simple code to implement I2C ,timer with PWM. But I have issue of memory overflow. I have enabled following:void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_I2C1_Init(voi...

NKaur.1 by Associate II
  • 4059 Views
  • 6 replies
  • 0 kudos

Resolved! Is it safe to remove STM32CubeIDE older versions?

Hello!My Ubuntu PC tells me that I'm running low on storage, and I would like to remove a few unused programs. I just installed STM32CubeIDE 1.7.0, but I noticed that in /opt/st, there are still older versions, 1.6.0 and 1.6.1. Is it safe to remove t...

PG.1 by Associate III
  • 1899 Views
  • 2 replies
  • 0 kudos

Resolved! Can't update Cube IDE

I cannot run updates from within Cube IDE.Help>Check For Updates throws the following error dialog:Unable to read repository athttps://sw-center.st.com/stm32cubeide/updatesite1/.Unable to read repository athttp://sw-center.st.com/stm32cubeide/eclipse...

Dfarr.1 by Senior
  • 4889 Views
  • 5 replies
  • 0 kudos

CubeIDE strange presentation of nested folder structure.

See the image. I can't figure out how I have done this, but my source folders appear like this, rather than in a hierarchy. When I open the folders in explorer, they are all nested as you would expect, folders inside folders. They are not folders wit...

DJC by Senior
  • 1198 Views
  • 0 replies
  • 0 kudos