STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1340 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 530 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Did not get SWV prints in STM32CubeIDE

Hii Everyone, I am trying to debug with SWO and SWV in STM32CubeIDE with NUCLEO-H753ZI. But, I am not getting any prints on SWV ITM Data console. As you can see all settings in the below attachments. My CPU system clock is running at 400Mhz. Anyone s...

SDTAN0907_0-1758694249404.png SDTAN0907_1-1758694368626.png SDTAN0907_2-1758694433406.png SDTAN0907_3-1758694547143.png
SDTAN0907 by Associate III
  • 3142 Views
  • 20 replies
  • 4 kudos

Serial Wire Viewer on STM32H7S3L8

Has anyone worked with the Serial Wire Viewer on an STM32H7RS board?We've been using it on a F7 board, without too much issue, but we are stuck on this new board. We've followed the usual steps :- Enable Serial Wire Viewer (SWV) in Debug configuratio...

PhilMaz_0-1736843286859.png PhilMaz_1-1736843475216.png PhilMaz_2-1736843517043.png
PhilMaz by Associate II
  • 2428 Views
  • 12 replies
  • 11 kudos

STM32CubeIDE 1.19.0 released

We are pleased to announce that the release 1.19.0 of STM32CubeIDE is available. What is new in 1.19.0: Microcontroller, microprocessor, and board lists aligned with STM32CubeMX v6.15.0:Added the support for STM32MP21xx microprocessors to the STM32MP...

Resolved! Not able to configure mbedtls in STM32CubeIDE

I want to use the rsa feature of mbedtls but when I uncomment #define MBEDTLS_RSA_C in the mbedtls_config file it is showing undefined reference to mbedtls_rsa_get_len, mbedtls_rsa_check_pub_priv, mbedtls_rsa_init, mbedtls_rsa_free and mbedtls_rsa_im...

Advait by Associate III
  • 1817 Views
  • 14 replies
  • 4 kudos

Resolved! Project Settings Missing Headers

I am currently following a tutorial on setting up micro-ros with STM32 uC's and for some reason, I can't seem to find a particular setting described in the steps.micro-ROS can be used with SMT32CubeIDE following these steps:Clone this repository in y...

msalazar_0-1759351791922.png
msalazar by Associate II
  • 715 Views
  • 3 replies
  • 1 kudos

Resolved! Very slow times for both STM32CubeIDE and STM32CubeMX

Hello, I am starting my project with CubeMX and CubeIDE right now and I am encountering massive time issues.For example it took almost 25 minutes to go from the IOC file to the generated code (throuh the autogenerating functionnality). It also took 3...

EliazLB by Associate III
  • 1155 Views
  • 6 replies
  • 3 kudos