cancel
Showing results for 
Search instead for 
Did you mean: 

STM's custom GUI not showing on Arch with GNOME 49 Wayland

SMT4497
Associate

Hi there,

So I'm using STM32CubeIDE as is the program we use in Embedded Systems subject at my university. I installed it on Arch with GNOME 49 Wayland (I know, they hate each other) and I'm passing the GDK_BACKEND=x11 environment variable. I've already fixed the debugger not having the proper libncurses version and now I can upload code to the board but I cant visualize IOC files, board selector, etc. Any help would be very appreciated.

Thanks in advance!

1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hello @SMT4497 

Unfortunately, STM32CubeIDE is not supported on the GNOME 49 yet. Below are the supported operating systems and architectures for STM32CubeIDE

• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 41
• macOS® 14 (Sonoma), macOS® 15 (Sequoia)

BR,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.