cancel
Showing results for 
Search instead for 
Did you mean: 

Very slow times for both STM32CubeIDE and STM32CubeMX

EliazLB
Associate III

Hello,

 

I am starting my project with CubeMX and CubeIDE right now and I am encountering massive time issues.

For example it took almost 25 minutes to go from the IOC file to the generated code (throuh the autogenerating functionnality). It also took 3 minutes and 45 seconds to build a basically empty program (except for the inits).

I'm running on CubeIDE v1.19 and CubeMX v6.15.

My laptop is Windows 11, I have 32 GB RAM, 13th Gen intel Core i7-13700H.

If you guys have any advice on how to work around it that would be great.

 

Thank you very much !

1 ACCEPTED SOLUTION

Accepted Solutions
EliazLB
Associate III

Ok it seems moving the project from my company's server to working directly on my laptop was the answer to my question ! 

Thanks for the answers guys

View solution in original post

6 REPLIES 6
Ozone
Principal III

I would recommend to at least run the task manager simultaneously, and check what application/process uses up most CPU time. Click on the "CPU" column to sort by CPU load.

I got a suspicion this is a virus scanner.

Erwan YVIN
ST Employee

Hello Eliaz ,

i recommend you to check on your windows :

  • Check your Windows defender (antivirus) in task manager during build process.
  • Proxy settings in your are in corporate company (some IP could be redirected and slows your PC)

On CubeIDE , there is windows defender exclusion check popup ;)

Help - Eclipse Platform

                                    Best regards

                                                 Erwan

                                   

When i just look at it without running anything on STM32Cube, it takes around 0.1% of CPU power and when running a build, it is from 0.2 to 0.5%. I had a spike to 1% but it lasted half a second.

The total use of CPU is from 10 to 15%.

Though I'm not very sure what to look for...

Could you indicate where to find the option you are talking about ? It seems that this is the problem I'm encountering.

Thank you !

Not sure if I made clear what I mean :

> For example it took almost 25 minutes to go from the IOC file to the generated code (throuh the autogenerating functionnality). It also took 3 minutes and 45 seconds to build a basically empty program (except for the inits).

Whatch the task manager during exactly those actions.
Perhaps try a "clean" before, or even a new project.

My company had mandated a certain McAfee virus canner for all their PCs, which brought down performance by 70..80%. And switched to an alternative only after massive complaints.

EliazLB
Associate III

Ok it seems moving the project from my company's server to working directly on my laptop was the answer to my question ! 

Thanks for the answers guys