STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

SDMMC on H7 using CubeIDE 1.8.0

Has anyone else had problems with the SDMMC peripheral on the H7 since the CubeIDE 1.8.0 Update. I have some old projects I went back to that had previously used this peripheral and now when mounting the SD Card I get a FR_NO_FILESYSTEM error. I have...

Jaboop by Associate II
  • 1749 Views
  • 2 replies
  • 0 kudos

How to input these instruments?

I tested the example "WiFiBasics" came from STM32CubeIDE on discovery board "B-U585I-IoT02A". The .elf file has been downloaded into board through STM32CubeProg, and when I opened PuTTY as it was told in example's "README", these was prompted:https:/...

MQi.1 by Senior II
  • 1210 Views
  • 1 replies
  • 0 kudos

How to convert MyLibName.a to MyLibName.bin?

Hello guys.I have an interesting project where I need to load user applications (binaries) from external flash memory (FATFS) into RAM and run them from there. Also, I want to use a static library (let's call it libAPI.a for example) that should be a...

0693W00000HnxjfQAB.png 0693W00000HnxkiQAB.png
Oleksandr by Associate III
  • 2652 Views
  • 5 replies
  • 0 kudos

STM32CubeIDE has a file containing viruses?

After we installed the STM32 Cube IDE program version 1.8.0 (the installation file is downloaded from STM site), our company Anti Virus software has detected that the program contains virus.From the report of the Anti Virus program, the file contains...

HNguy.18 by Associate
  • 1476 Views
  • 1 replies
  • 1 kudos

BDMA -Availability depends on devices.

hello ı use stm32h723zg and ı use bdma for adc3 , I was wondering if bdma can be used with adc3. I looked in the reference guide but couldn't find it. I will be glad if you help.

0693W00000HnnvbQAB.png