cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE missing pin labels

HZz.1
Associate

using: NUCLEO-H745ZI-Q board, STM32CubeIDE: Version: 1.8.0 Build: 11526_20211125_0815 (UTC)

I am new to STM32 and trying to do a simple led/gpio test.

can't identify a pin since there is no label that converts from port and pin, saw at some tutorials they use the labels that are at the ioc file:

example:

PB0.GPIO_Label=led_h

PB14.GPIO_Label=LD3 [Red Led]

at STM32CubeIDE when searching or ctrl+space it seems that there is no labels only GPIOA etc. and GPIO_PIN_0 etc.

how can I identify the correct way to interface to a pin?

Thank you,

Hanan

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

You need to assign pins to the core that you want to use them on. If you do so, the port/pin definitions will appear in the main.h file for that core.

Right click the pin and assign it to a core.

0693W00000HoqoBQAR.png

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

You need to assign pins to the core that you want to use them on. If you do so, the port/pin definitions will appear in the main.h file for that core.

Right click the pin and assign it to a core.

0693W00000HoqoBQAR.png

If you feel a post has answered your question, please click "Accept as Solution".
HZz.1
Associate

It worked, thank you