STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1417 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to publish an STM32CubeIDE project on Github

I'd like to publish an STM32CubeIDE project on Github, but I haven't found a method that works. I'd like to be able to upload my project from STM32CubeIDEVersion: 1.8.0Build: 11526_20211125_0815 (UTC)OS: Linux, v.5.13.0-28-generic, x86_64 / gtk 3.24....

CKugl.1 by Senior II
  • 3176 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE depends on discrete GPU on macOS

Hi Community, ​The env is: STM32CubeIDE 1.8.0, macOS 10.15.7, MBP16-2019​When STM32CubeIDE is running, the OS switches to discrete GPU and eat about 30W totally(with integreted GPU only 10W is needed). The battery is running low fast.​I force switch ...

XWang.5 by Associate II
  • 708 Views
  • 0 replies
  • 0 kudos

Resolved! I don't understand why STM32CubeIDE give me this syntax error. How do you access to array that are inside a struct?

typedef struct{ uint8_t data[10]; uint8_t time[10]; uint8_t description[10];} FileString;FileString Datalogger_FileString;Datalogger_FileString.data[0]=0; //ERROR: expected '=', ',', ';', 'asm' or '__attribute__' before '.' tokenWhat do I should do t...

William F by Associate II
  • 3667 Views
  • 2 replies
  • 1 kudos

Resolved! STMCubeIDE gives the message "Break at address "0x1fff5162" with no debug information available, or outside of program code."

Hello. I work in CubeIDE 1.9.0 with the stm32f429i-disco device. The problem arises about firmware and debugging. I made a simple example to check. During debugging, strange behavior was noticed when executing HAL_Delay (line 95). When executing Step...

DalOpez by Associate II
  • 10184 Views
  • 3 replies
  • 0 kudos

How to run "Percepio Tracealyzer" in CubeIDE?

From "Eclipse Marketplace" I installed "Precepio Trace Exporter for STM32CubeIDE 1.1.4" see screen.And according to this video https://youtu.be/nw3sEkfbTI0?t=95I have to insert some files in to my project of FreeRTOS.From where I can get these files?...

0693W00000Lvq30QAB.png 0693W00000LvpsRQAR.png
DK.7 by Senior
  • 1203 Views
  • 0 replies
  • 0 kudos