STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1415 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Impact of CubeIDE update on existing source code

Hello,there are so many topics out there about "stuff not working after CubeMX / CubeIDE update", so I wonder how that could impact my "workflow".I'm using CubeMX only as a starting point, and as soon as I have some basic stuff running (usually UART ...

LCE by Principal II
  • 2329 Views
  • 4 replies
  • 0 kudos

Resolved! Uart Circular buffer , Error while building using Nucleo 429zi Just did what is in the video in the link https://controllerstech.com/ring-buffer-using-head-and-tail-in-stm32/ The error is as shown in the details

arm-none-eabi-gcc -o "Uart_Ring_Buffer.elf" @"objects.list"  -mcpu=cortex-m4 -T"C:\Users\User\STM32CubeIDE\workspace_1.8.0\Uart_Ring_Buffer\STM32F429ZITX_FLASH.ld" --specs=nosys.specs -Wl,-Map="Uart_Ring_Buffer.map" -Wl,--gc-sections -static --specs=...

RKore.1 by Associate II
  • 2891 Views
  • 5 replies
  • 0 kudos

Resolved! How do I update the HAL on an existing STM32G0 project?

I have a Nucleo-32 STM32G031K8. STMCubeIDE was installed around March 1. I have been trying to debug and getting slave code working to respond to HAL_I2C_Mem_Read_DMA() and HAL_I2C_Mem_Write_DMA() commands from another STM32G032K8. When I looked at...

KiptonM by Lead
  • 3521 Views
  • 5 replies
  • 0 kudos