STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1555 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIde hangs during startup after an update

Hi,Yesterday I updated my STM32CubeIde. Today it hangs during start.The message windows do not respond to any actions (see printscreen)In the log files "E:\work\STM32Cube\.metadata\.ide.log" I have the following entry:2023-02-01 08:00:55,772 [INFO] A...

0693W00000Y9ghBQAR.png
Mat1 by Associate III
  • 2145 Views
  • 4 replies
  • 0 kudos

STM32 IDE bug while using target selection

If you try to create a new project via target selection and try to search for the commercial part number, the cursor moves to the search bar immediately below each time you try to type a character.Details from about page:Version: 1.11.2Build: 14494_2...

PMarz.2 by Associate II
  • 3099 Views
  • 6 replies
  • 0 kudos

STM32CubeIDE Debugger operation seems to override a COM Port

Hi. I am attempting to get a basic USB_FS to communicate between my STM32 Board (STM32756-EVAL) and my PC, through PuTTY. The following are the configs on my PuTTY connection.And the following is my code in main.c:#include "main.h" #include "i2c.h" #...

0693W00000Y9LmUQAV.png 0693W00000Y9Lw5QAF.png 0693W00000Y9LxXQAV.png 0693W00000Y9LxcQAF.png
OIp.1 by Associate III
  • 3165 Views
  • 5 replies
  • 1 kudos

HardFault

Hi, can i know why i got this error? i click on fault editor but it say no address 0x00. btw this is my hardfault error. i don't know how to solve it 

0693W00000Y9Y1qQAF.png 0693W00000Y9XwWQAV.png 0693W00000Y9Y2KQAV.png
Angle by Associate II
  • 1540 Views
  • 1 replies
  • 0 kudos

I2S_DMAResume does not Sync in Slave mode. (CubeIDE)

I am using STM32F446 Nuclero and STM32CubeIDE.​I wrote a loopback code from I2S_ADC (PCM1808PWR) to internal DAC.MCU is slave mode (external clock to IS2_CKIN).I works fine. ​However, when I try to "Pause DMA" and "Resume DMA", I2S of MCU does not sy...

KAJIK.1 by Associate III
  • 3375 Views
  • 4 replies
  • 0 kudos

How to configure external clock in STM32CubeMx

According to the data sheet for this device, I should be able to attached an external High speed crystal instead of using the HSI RC. However, I can't seem to figure out how to do this using the STM32CubeMX utility.

JWill.10 by Associate II
  • 2408 Views
  • 2 replies
  • 1 kudos