Skip to main content
SMt.1
Visitor II
February 1, 2023
Solved

How can I transfer a project from STM32CubeIDE to IAR Embedded Workbench?

  • February 1, 2023
  • 1 reply
  • 3118 views

..

This topic has been closed for replies.
Best answer by S.Ma

I've done the opposite...

Maybe first make a skeleton project with CubeMX which generates the IAR EWARM project file, possibly with the right target STM32 and package, and cloctree etc... depending on how much you need.

Then generate the code . Open IAR and check the project compile.

Add your source files in the skeleton project folders, then on IAR, add them.

Remember to select the target, the compile options, the compiler search directories and the compiler default passing named arguments. These are the things not to forget.

Also make sure there are no #pragma compiler specific. Think also memory mapping, stack size, etc...

If things are not too complex, you'll get a build with few errors and warnings to cleanup.

Mileage varies, depending on the project complexities...

1 reply

S.Ma
S.MaBest answer
Principal
February 1, 2023

I've done the opposite...

Maybe first make a skeleton project with CubeMX which generates the IAR EWARM project file, possibly with the right target STM32 and package, and cloctree etc... depending on how much you need.

Then generate the code . Open IAR and check the project compile.

Add your source files in the skeleton project folders, then on IAR, add them.

Remember to select the target, the compile options, the compiler search directories and the compiler default passing named arguments. These are the things not to forget.

Also make sure there are no #pragma compiler specific. Think also memory mapping, stack size, etc...

If things are not too complex, you'll get a build with few errors and warnings to cleanup.

Mileage varies, depending on the project complexities...