STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1555 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Ethernet with Nucleo-144 STM32F746GZ did not work with STM32CubeIDE 1.10.1 and STM32F7 library 1.70.1. The CubeMX is 6.6.1.2.

The Nucleo-144 F746GZ board worked fine with legacy Ethernet FW from System Workspace (as well as demo FW from System Workspace). I have added PG12 for Phy Reset however I am unable to get ethernet up via a twisted ethernet connection to the laptop. ...

Riscy by Senior
  • 6086 Views
  • 16 replies
  • 1 kudos

Resolved! How to add .o file in STM32 cube IDE

Hello all,I have referred the STM32cubeIDE user manual and found the procedure to add the .o file to the project.I want to call a function from the added .o file.But I get the following error.../Core/Src/main.c:130:3: warning: implicit declaration of...

Aarra.1 by Senior
  • 2848 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 IDE type and list down function/variable suggestion list

I saw some tutorials with STM32 IDE 1.11.0, > When typing for the variable or function name, it makes a list and selected if found.and I don't see it doing that; where is the configuration in preference top enable it or was is it from the plugin fea...

Riscy by Senior
  • 4345 Views
  • 1 replies
  • 0 kudos

STM32 IDE failed to evaluate expression glitch

Hello.Whenever I try to debug my file and use the live expressions tab, it used to work earlier and give me values but now it's just showing me failed to evaluate expression eve though I have correctly defined the variable. Please help with a fix. I ...