STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1555 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 589 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32F103C8T6 HardFault immediately after debugging starts.

Hi. I have some strange error when debugging code at my STM32F103C8T6 BluePill board.When I start debugging, everything seems fine (the debugger connects to the target, erases it, downloads firmware, and verifies it successfully). But instead of jump...

0693W00000aIDJ1QAO.png 0693W00000aIDJBQA4.png
AMelk.1 by Associate II
  • 4384 Views
  • 3 replies
  • 3 kudos

Resolved! STM32CUBEIDE add SDK files

Hi all, i am facing a problem with stm32cubeide. i copied and paste a SDK folder to project folder and it is showing there in project directory in stm32cube ide. (refer 1.png)then i added header files paths through project > properties > c/c++ genera...

sanju by Senior
  • 8127 Views
  • 4 replies
  • 1 kudos

ST-link not detected and Drivers not listed

I was trying to run a program on STM32CubeIDE1.11.2 and the board lost connectivity. When checking the device manager, it is now listed as unknown usb, as well as stm drivers not being listed when trying to manually assign it. Additionally i tried un...

DUlli.1 by Associate II
  • 3088 Views
  • 6 replies
  • 0 kudos