STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1403 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Explanation field to CubeIDE

Feature request to STM32 CubeIDE.ST, please add a possibility to add user explanation text to peripheral configurations. It is neccessary because the configuration, especially numbers, are not always self-explaning. A text field where to write explan...

MikkLeini_0-1690122823653.png

STM32F1xx DALI slave interface

Hi everyone,I downloaded the DALI Slave Library from here: https://www.st.com/en/embedded-software/stsw-dali001.html and now I am trying to run the demo code on my STM32F103C8T6.The problem I am encountering is that the source code has a few commands...

Live Expression values are shown wrong

The variables in the live expression are showing incorrect values. Previously, they showed the correct values, but after making several changes to the .ioc file and the code, the values are now displayed incorrectly.Below, I have provided some pictur...

Screenshot (963).png Screenshot (964).png Screenshot (965).png Screenshot (967).png
Anistus by Associate
  • 1274 Views
  • 0 replies
  • 1 kudos

Resolved! Is STM32CubeIDE newlib with FreeRTOS now really thread safe?

I'm using STM32Cube IDE with FreeRTOS. The Errata for STM32CubeIDE 1.7.0 state "70505 Implemented a newlib-malloc solution that is thread safe by default."Is newlib truly thread safe now? As far as I can tell, when building a project in STM32CubeIDE...

msch by Associate III
  • 15291 Views
  • 11 replies
  • 1 kudos

Resolved! easiest way to share data between cores in STM32H745

Hello @RMcCa I am working on the same area where i want to write variable in shared memory of SRAM4 via M4 and to read from M7. I have gone through your post Best/easiest way to share data between cores in ST... - STMicroelectronics CommunityCould yo...

Nsg1987 by Senior
  • 3874 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE Debug not recognized stlink v2

Hello everyone,I trying debug a project,bu t when I connect Scan my ST-Link in CubeIDE got wrong S/N and error when start.In ST-Link Utility gets rigth S/N.Any solve for this case?I have tried ohter cable, drivers and etc...  

MuriloCF_1-1690383624062.png
MuriloCF by Associate II
  • 5872 Views
  • 7 replies
  • 0 kudos

Resolved! %% Formatter Bug - snprintf

HARDWARE/SOFTWARE INFOHardware: NUCLEO-WB55RG Dev Board Device Page STM32CubeIDE:    Version: 1.13.0                               Build: 17399_20230707_0829 (UTC)GGC Assembler All Options: -mcpu=cortex-m4 -g3 -c -x assembler-with-cpp -mfpu=fpv4-sp-d...

mikerr by Associate
  • 2921 Views
  • 1 replies
  • 1 kudos

Memory Protection unit

I am new to stm32cubeide. I need to configure memory protection unit on stm32f407g-disc1 discovery board using stm32cube ide.

Nehal by Associate
  • 1505 Views
  • 1 replies
  • 0 kudos