STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 596 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Compile error with InfraredPD_CM0P_wc32_ot.a library.

Hello!We have a project for STHS34PF80TR IR sensor.We are setting the library "InfraredPD_CM0P_wc32_ot.a" in project options, but following compiler error is generated:c:\st\stm32cubeide_1.11.2\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externalto...

LMehm by Associate III
  • 1730 Views
  • 2 replies
  • 0 kudos

stm32cubeide crashes on ubuntu after upgrade

Hello,I upgraded my IDE to 1.13.0 yesterday on Ubuntu 22.04 and now it crashes just after startup. I can see no error message on the console.Even the previous version 1.12.x now crash.What information do you need from my system to pass on?Kind regard...

PGild.1 by Associate III
  • 1493 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE examples for Nucleo-F446ZE

I know I can load Nucleo-F446ZE examples from the STM32CubeIDE, but what I find really annoying is the the examples provided are made in SW4STM32 IDE .To me it is very strange that while STM is promoting their STM32CubeIDE, I have to learn the SW4STM...

Copeland by Associate II
  • 1494 Views
  • 1 replies
  • 0 kudos

Resolved! how to change output pin to pwm pin

hello guys i am new to stm,i am using stm32103 and stmcubeide ,my question is very basic ,i know how to initialize a pin as an output pin or as a pwmpin but i donot know that how to change an output pin into a pwmoutput pin and then again convert tha...

ahmash by Associate III
  • 3696 Views
  • 2 replies
  • 2 kudos

Resolved! PH3-BOOT0

Hi,I am using STM32U585RIT6 MCU & I planned to flash the firmware through SWD and onboard debugger module (STLINK-V3MODS) through VCP.I am having confusion in configuring the PH3-BOOT0 pin.Should I connect it to 5V or GND.Or shall I make it No connec...

mkm by Associate
  • 1837 Views
  • 1 replies
  • 1 kudos

Error in initializing ST-Link

Hello Sir,     I'm new to this STM 32 environment. I'm using Nucleo F429ZI board when I try to debug the board it shows the following error."Error in final launch sequence:Failed to execute MI command:target remote localhost:61234Error message from d...

MA by Associate II
  • 2919 Views
  • 5 replies
  • 0 kudos

B-L475EIOT01A1 Example Code

Hi,New to STM32 tooling and am trying to find example source code for the B-L475E-IOT01A1 board.Nothing seems to pop up on the Example Selector of the Target Selector window and there doesn't seem to be any downloads for examples from the product pag...

Resolved! FreeRTOS: Only one of two tasks are occurring

Hello,I am utilizing a FreeRTOS system on the STM32H725AGI6 in my software with two purposes:- Run a task that handles the TouchGFX process to operate an LCD display- Run a task that handles a BLE process (Which utilizes theBlueNRG-M0A)I have tested ...

KMew_7-1691714181441.png KMew_0-1691713695694.png KMew_1-1691713715092.png KMew_2-1691713738276.png
KMew by Senior III
  • 5878 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.