STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

TICK_INT_PRIORITY affected by enabling TRACE outputs

I'm working on a project based on a STM32F107VC using CubeMX V6.3.0 using STM32Cube FW_F1 V1.8.4. In this project, the Timebase Source is set to TIM7. In the original project state, the code generation defines TICK_INT_PRIORITY to 0U.We need to remap...

JPerr.2 by Associate III
  • 1260 Views
  • 0 replies
  • 0 kudos

Resolved! [STM32CubeIde] No auto-completion in expressions window

Hello,I have no auto-completion in the expressions and live expressions windows. This is quite annoying because the complete variable names have to be typed in.In the editor window the auto-completion works fine.I know it from other Eclipse based IDE...

ThorstenO by Associate II
  • 2226 Views
  • 2 replies
  • 0 kudos

Problems with importing OTA Software Pack

Hello!I am doing a Bluetooth OTA application and noticed there is an OTA software package.STMicroelectronics X-CUBE-BLEMGR   ->BLE_Features  ->Miscellaneous  ->WB_FirmwareUpdate / OtaBut when I select the "WB_FirmwareUpdate / Ota", then a warning wit...

DenDanne_0-1694022695982.png DenDanne_1-1694022910931.png
DenDanne by Associate II
  • 2592 Views
  • 3 replies
  • 0 kudos

Resolved! Can't set preemption priority for ethernet global interrupt

Hi,I am making LwIP + TouchGFX project on STM32H750B-DK following the next tutorial:https://github.com/GrzHeller/STM32H750B-DK_TouchGFX_FreeRTOS_MQTT_Example/blob/main/README.mdWhen setting ethernet settings in .ioc I can enable ethernet global inter...

eth.PNG
AK16 by Associate II
  • 2014 Views
  • 1 replies
  • 0 kudos

Resolved! 2D-FFT rfft and cfft functions

I have a 2D array input buffer. so, what is the correct way to implement the rfft and cfft functions?float fftIn[16][512] is my input. So, I applied for a loop like below:arm_rfft_fast_init_f32(&fftHandler, 512); for(int d =0; d<16; d++){arm_rfft_fas...

AKhot.1 by Senior
  • 4207 Views
  • 3 replies
  • 1 kudos