Associate
April 3, 2023
Question
Debugging with GDB server localhost doesn't work
- April 3, 2023
- 3 replies
- 3504 views
STM32CubeIDE for MAC Version: 1.12.0
Just installed the tools and connected an STM32 Nucleo 144 for the first time.
After connecting it, a ST-Link upgrade window popped up about updating the firmware of the board which I did. Got the Upgrade successful message, but if I open this window again and choose the Open in update mode, the following option still shows up and lets me upgrade again.
After creating a test project, when I try to start Debugging, it fails due to no connection to port 61234. I'm using the Autostart Local GDB Server option.
I tried changing the port number and also the ST-Link Open OCD but still can't get the debugger to work
[0.000] initConfigParams(): Configuration flags start
[0.000] initConfigParams(): external-init false
[0.000] initConfigParams(): pend-halt-timeout (null)
[0.000] initConfigParams(): halt false
[0.000] initConfigParams(): config-file ""
[0.000] initConfigParams(): persistent false
[0.000] initConfigParams(): +log-file "/Users/Michael/Desktop/Embedded udemy/MCU1-Course/MCU1/001HelloWorld/Debug/st-link_gdbserver_log.txt"
[0.000] initConfigParams(): +log-level 31
[0.000] initConfigParams(): +port-number 61234
[0.000] initConfigParams(): +verbose true
[0.000] initConfigParams(): refresh-delay 15
[0.000] initConfigParams(): +verify true
[0.000] initConfigParams(): +swd true
[0.000] initConfigParams(): +swo-port 61235
[0.000] initConfigParams(): cpu-clock 8000000
[0.000] initConfigParams(): swo-clock-div 128
[0.000] initConfigParams(): initialize-reset false
[0.000] initConfigParams(): debuggers false
[0.000] initConfigParams(): serial-number ""
[0.000] initConfigParams(): +apid 0
[0.001] initConfigParams(): +attach true
[0.001] initConfigParams(): shared false
[0.001] initConfigParams(): erase-all false
[0.001] initConfigParams(): memory-map ""
[0.001] initConfigParams(): ext-memory-loaders false
[0.001] initConfigParams(): extload_init (null)
[0.001] initConfigParams(): extload (null)
[0.001] initConfigParams(): +stm32cubeprogrammer-path "/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_2.0.600.202301161003/tools/bin"
[0.001] initConfigParams(): temp-path ""
[0.001] initConfigParams(): preserve-temps false
[0.001] initConfigParams(): frequency 0
[0.001] initConfigParams(): licenses false
[0.001] initConfigParams(): ignore-rest false
[0.001] initConfigParams(): version false
[0.001] initConfigParams(): help false
[0.001] initConfigParams(): Configuration flags end
[0.001] init(): STMicroelectronics ST-LINK GDB server. Version 7.3.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
[0.011] openDevice(): COM frequency = 4000 kHz
[0.011] openDevice(): Target connection mode: Attach
[0.018] readFromTarget(): Reading ROM table for AP 0 @0xe00fdfd0
[0.042] reset_hw_wtchpt_module(): Hardware watchpoint supported by the target
[0.057] initContext(): ST-LINK Firmware version : V2J41M27
[0.057] initContext(): Device ID: 0x449
[0.061] initContext(): PC: 0x0
[0.070] Device_GetStatus(): ST-LINK device status: RUN_MODE
[0.071] initContext(): ST-LINK detects target voltage = 3.24 V
[0.072] initContext(): ST-LINK device status: RUN_MODE
[0.072] initServerContext(): ST-LINK device initialization OK
[0.072] pollAndNotifyRun(): Stm32Device, pollAndNotify running...
[0.076] updateState(): SwvSrv state change: 0 -> 1
[0.076] WaitConnection(): Waiting for connection on port 61235...
[0.077] WaitConnection(): Waiting for connection on port 61234...
[2.268] stop(): Stopping port 61234
[2.268] WaitConnection(): Received stop for port 61234, not accepting new connections.
[2.268] deInit(): GdbSrv, deInit entry.
[2.268] deInit(): GdbSessionManager, deInit entry.
[2.343] deInit(): GdbSessionManager, deInit exit
[2.343] deInit(): SwvSrv deInit entry
[2.343] stop(): Stopping port 61235
[2.448] WaitConnection(): Received stop for port 61235, not accepting new connections.
[2.448] deInit(): SwvSrv deInit exit
[2.448] closeDevice(): Stm32Device, closeDevice() entry
[2.449] pollAndNotifyRun(): Stm32Device, pollAndNotify stopped
[2.455] closeDevice(): Stm32Device, closeDevice() exit
[2.455] deInit(): Stm32Device, deInit success
[2.455] deInit(): GdbSrv, deInit exit.